2019-10-23 2:17 AM
Hello,
I would like to implement TouchGFX on a custom board equipped of a STM32L4R9 microcontroller, but I can't find the TouchGFX framework neither on the CubeMX interface nor on the CubeIDE interface, at the topic "MIDDLEWARE/GRAPHICS ..."
Please help for implentation !
And yet, ST Microelectronics clearly mentions that Touch GFX is supported on STM32L4+ family.
It's not very friendly for the developpers to observe that the "marketing speech" doesn't match the "technical" one !!
Please update CubeMX and/or CubeIDE to be able to use the FULL TouchGFX functionalities on STM32L4+ microcontrollers family.
Thank you.
2019-10-23 7:38 AM
You can and you can't. Let me clarify.
/Martin
2020-01-27 5:33 AM
Hello Martin,
we are currently in a situation where we are using a STM32L4R9i-Discovery board and are developing a GUI using touchGFX.
But we do not know how we can integrate the touchGFX portion into the Cube IDE. Any help would be very much appreciated. Is there an documentation which would guide us through the proces. So far I only find docus/videos that are setting up touchGFX in the middleware section of CubeIDE. And if i undestand you right does not work with the STM32L4R9i-Discovery.
best regards
joerg