2018-12-26 8:33 PM
Hello.
Im trying to flash evaluation board STM32H743I-EVAL with help of touchgfx designer 4.10.0.
In the simplest case i create project with application template ST STM32H743I EVAL and without any elements (no backgrounds, buttons etc.).
But when i try to flash (button "run target"), i havethis:
make -f target/gcc/Makefile -j10 flash
An error occured during flash. Please make sure you have the right target connected.
Converting images
STM32 ST-LINK CLI v3.3.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN: 0672FF323338424E43254935
ST-LINK Firmware version: V2J32S22 (Need Update)
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 3.2 V
Connection mode: Normal
Reset mode: Hardware reset
Device ID: 0x450
Device flash Size: 2048 Kbytes
Device family: STM32H7xx
Loading file...
Flash Programming:
File : build/bin/target.hex
Address : 0x08000000
The elf loader file is not accessible.
MCU Reset.
target/gcc/Makefile:389: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 12
target/gcc/Makefile:77: recipe for target 'flash' failed
make: *** [flash] Error 2
And i tried to update ST-LINK firmware, it doesnt help and debug log still displays the message "need update".
Help me pls to fix my problem, how to flash stm32h743i?
2018-12-27 9:51 AM
Hi. Can you share the details of which ST-LINK update you have applied and tested?
2018-12-27 7:48 PM
STM32 ST-LINK Utility v4.3.0.0
STLinkUSBDriver.dll v5.1.0.0
ST-LINK_CLI.exe v3.3.0.0
Firmware Version: V2.J32.M22 STM32 Debug+Mass storage.
But i think that problem in generating some memory files, because when i try to flash firmware from IAR,
it shows error "FlashSTM32H7xxx_CM7.flash file was not found". Way to this file is containing in "QSPI.board" file. And "FlashSTM32H7xxx_CM7.flash" is not present in EWARM folder,
unlike "QSPI.board". When i try to use default IAR's flashloader files, it flashes, but do it wrong.
And for example look at comparsion generated STM32F7 and STM32H7 folders. STM332F7 board file contains ways to ".flash" files, which are presented in IAR folder.
2019-01-01 6:21 AM
Which ST-LINK update have you applied?
Can you try again after upgrading the following tool?
STSW-LINK009 2.0.1
2019-01-01 6:24 AM
Also, your CLI version is old.
STM32 ST-LINK CLI v3.3.0.0
Current version is posted here:
https://www.st.com/en/development-tools/stsw-link004.html
Current version is 4.3.0.
2019-01-08 9:47 PM
2019-01-08 11:30 PM
Hi @feelingoflight,
It does look like an incorrect version. When you call make with the "flash" option, it simply makes a call to the ST-Link CLI and if your version does not have the right support (both internal flash and external) you'll get that message "No elf loader found".
Could you try showing me the "About" window from your ST-Link GUI ?
2019-01-08 11:31 PM
Could you try programming your board from the GUI to see if you get the same error there? I seem to remember having issues with H743I-EVAL and ST-Link.
Moving to STCubeProgrammer resolved my/our issues here. Try it out!
2019-01-09 12:32 AM
2019-01-09 12:36 AM
Yeah, i tried to flash file target.hex from application/build/bin from st-link utility and from stm32cubeprogrammer, it works, but with some bugs. For example when i add scalable image on screen it flashes wrong and nothing works.
Also i would like to generate hex files from IAR, not from designer or cmake.
Thanks for help, maybe i need to wait more stable version touchgfx.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.