cancel
Showing results for 
Search instead for 
Did you mean: 

How to change screen when clicking animation?

jackson.kang
Associate II

I made the animation run as TouchGFX Designer on the STM32F769I-DISCO board.

When i click the animation, I want to do another action(change the screen)

what should i do?

It would be better if there were related links or samples.

4 REPLIES 4
Alexandre RENOUX
Principal

Hello jackson.kang,

I'm not sure I follow what you are asking for, so if I don't answer correctly, could you provide more information (maybe some screenshot) ?

If you want to trigger an action when the button is clicked, simply use the Interaction tab in the Designer and create your interaction.

You can have a look at this page ("Step 4" section) : https://support.touchgfx.com/docs/tutorials/tutorial-02

/Alexandre

jackson.kang
Associate II

v

Thank of your answer!

I tested the "change screen" with "Animation is done" and "Button is clicked" in the trigger of the interaction​.

However, i want to do the change screen when i click on the animation while the animation is running.​0693W000008yq6hQAA.png0693W000008yq6cQAA.png

Alexandre RENOUX
Principal

Hello jackson.kang,

Could you enclose your project in this thread ? Or maybe if it's something you don't want to disclose, you can send it to me by private message.

/Alexandre