cancel
Showing results for 
Search instead for 
Did you mean: 

how can I port TouchGFX on FMC displays

SEMad
Associate III

Hi.

I am using a ili9488 display along side with stm32h7b0vbt6.

the lcd driver works fine... but touchgfx wont work.

0693W00000NrDEdQAN.png(FMC bank mapping is swapped.)

first:

"TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect)" function is the only function that should be edited? and how?

I had a look on l496-disco example but it seem it was created by old versions of touchgfx. some codes was different from my project...

second:

is it possible to use the GRAM as frame buffer?

thanks.

1 REPLY 1
Yoann KLEIN
ST Employee

Hello @SEMad​ ,

What do you mean exactly with "TouchGFX won't work" ? Is the designer not generating code or is it not running or target ?

And just to be sure, which version of the designer are you using ?

Thank you,

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX