Skip to main content
Associate
September 9, 2024
Solved

I replaced the stm32f407ve chip on my board but it didn't work

  • September 9, 2024
  • 6 replies
  • 1269 views

on my mks monster8 v2 3d printer control board using stm32f407ve chip it was damaged specifically gnd pin and vcc pin are connected, i bought another chip and soldered it to the board, however when plugging in usb it does not recognize com port, i tried connecting with my stlink v2 it still displays the necessary parameters and can read and write, i loaded blink led program and it works however when loading printer firmware specifically marlin it does not work and usb connected to computer does not recognize com port

This topic has been closed for replies.
Best answer by Tesla DeLorean

The failure is perhaps more involved. You'll need to get a schematic and work through the circuit. You've likely damaged the supply, check voltages and components in the path.

Perhaps find a repair technician familiar with the board, or find forums dedicated to support of the board,

6 replies

mƎALLEm
ST Technical Moderator
September 9, 2024

Hello @duong and welcome to the community;

As you have replaced the MCU, double check the hardware, mainly the USB part.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
duongAuthor
Associate
September 9, 2024

I checked the hardware again, the two pins d+ and d- of the usb are connected directly to the microcontroller through the two corresponding pins PA12 PA11, it is soldered exactly according to the pin out of the board manufacturer

 

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
September 9, 2024

The failure is perhaps more involved. You'll need to get a schematic and work through the circuit. You've likely damaged the supply, check voltages and components in the path.

Perhaps find a repair technician familiar with the board, or find forums dedicated to support of the board,

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
duongAuthor
Associate
September 10, 2024

maybe you are right, i measured the resistance on pin pa12 with gnd, the value is 6.5 ohm and pa11 with gnd, the resistance is up to Mohm

duongAuthor
Associate
September 10, 2024

pa12 is 6.5 kohm

 

duongAuthor
Associate
September 15, 2024

i replaced a new chip loaded the program with st link and tried with the code the led blinking works fine but still can not connect to usb, i hold boot 0 and power on bootloader mode still works, did i forget some step, please help me