2021-12-15 01:35 AM
I need to skip the upper row and lower row and print the characters.
Solved! Go to Solution.
2021-12-17 03:51 AM
Thank you for suggestions @Andrew Neil and @Community member. I got the issue it was some address problem I Solved it.
2021-12-15 06:08 AM
Show us what do you have so far - both hardware and software.
What do you mean by "skip the upper row and lower row"?
JW
2021-12-15 06:29 AM
In addition to what @Community member said, have you looked on the Avago site for application notes, examples etc?
Have you searched for other examples?
Note that Avago is now Broadcom: https://www.broadcom.com/products/leds-and-displays/smart-alphanumeric-displays/parallel-interface/hdsp-2533
2021-12-15 08:30 PM
Hi waclawek and andrew please see attached pdf and actual i need to print as picture show im following as per pdf but udc(user defined code) address start with 80 upto 8f in 1st address i can store remaining is not working. im communicating display with parallel bus using stm32 controller.
2021-12-17 03:51 AM
Thank you for suggestions @Andrew Neil and @Community member. I got the issue it was some address problem I Solved it.
2021-12-17 04:47 AM
jolly good - glad you fixed it.
Now please mark the solution: