2022-05-17 12:32 PM
If so, can you tell me what LCD you targeted?
Solved! Go to Solution.
2022-05-27 5:31 AM
Hello,
The LCD used in LCD example available in STM32CubeWB package is the same than on 32L476GDISCOVERY and 32L152CDISCOVERY boards. The reference of this screen is GH08172T.
Best Regards
2022-05-24 7:12 AM
Hello,
You can look LCD example available in STM32CubeWB package to see how to used the LCD interface on the STM32WB55XX. More information about LCD interface are available in the reference manual.
Best Regards
2022-05-24 7:41 AM
First of all, thank you for your answer.
I did find the resources you have indicated. I do like the way that ST makes it fairly easy to find the chips. Unfortunately, everything indicates a "24 segment, 4 common" LCD without indicating a specific part number. Looking at Digikey and Mouser, I am unable to find an LCD that is compatible with the part.
So, my question still stands (rephrased for clarity), what LCD part number did you target if you used the LCD interface of the STM32WB55XX?
2022-05-27 5:31 AM
Hello,
The LCD used in LCD example available in STM32CubeWB package is the same than on 32L476GDISCOVERY and 32L152CDISCOVERY boards. The reference of this screen is GH08172T.
Best Regards