Guides for using TouchGFX 4.10 with CubeMX 5.0 & Known limitations.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-17 4:48 AM - edited ‎2023-11-20 3:13 AM
Note:
Recommended to use latest X-Cube-TouchGFC 4.13 release. Can be downloaded here: https://www.st.com/content/st_com/en/stm32-graphic-user-interface.html
Documentation link: https://touchgfx.zendesk.com/hc/en-us/sections/360003093319-TouchGFX-Releases
Guides for using TouchGFX with CubeMX & Known limitations.
This forum post will be updated along with newly acquired information regarding the interoperability of CubeMX and TouchGFX.
TouchGFX knowledge base article overview:
Link: https://touchgfx.zendesk.com/hc/en-us/articles/360020001492-Getting-Started-with-CubeMX-and-TouchGFX
This guide gives a general introduction to the workflow of creating an application for graphics with CubeMX and TouchGFX.
There are two ways of getting started with graphics on a ST discovery board
- 1: In TouchGFX Designer select one of the CubeMX enabled Application Templates and start developing graphical applications
- 2: In CubeMX select the desired STBoard from the board selector and add the TouchGFX graphic component.
Please note, that CubeMX does not provide implementation for BSP layer, these files are located in the respectively STM32Cube package for the selected STBoard.
https://touchgfx.zendesk.com/hc/en-us/articles/360019884752-Configuring-STM32F746G-DISCO
This guide describes how to enable TouchGFX graphics on a STM32F746G-DISCO board stating from the STBoard selector in CubeMX.
Opening from TouchGFX Designer, please note that the Application Template contains 2 versions. Version 2.0 is advised.
https://touchgfx.zendesk.com/hc/en-us/articles/360020001992-Configuring-STM32F7508-DISCO
This guide describes how to enable TouchGFX graphics on a STM32F7508-DISCO board stating from the STBoard selector in CubeMX.
https://touchgfx.zendesk.com/hc/en-us/articles/360020208091-Configuring-STM32F769I-DISCO
This guide describes how to enable TouchGFX graphics on a STM32F769I-DISCO board stating from the STBoard selector in CubeMX.
Opening from TouchGFX Designer, please note that the Application Template contains 2 versions. Version 2.0 is advised.
Additional known limitations / updates:
IDEs / Compilers:
IAR is currently working best out-the-box.
More work is needed when using Keil, Atollic, SW4STM32.
Missing BSP Layer
Generating a TouchGFX project from CubeMX, drivers for external components like touch controller and QSPI flash is missing.
TouchGFX Designer error message.
Starting from TouchGFX Designer with an Application templates based on a CubeMX project, the following message appears “Project was modified outside externally�?.
TouchGFX Designer renames the CubeMX and EWARM project files to match the name of the TouchGFX project file.
TouchGFX 4.10
The newest released TouchGFX version is 4.10, available in F4 and F7 Cube packages, and TouchGFX Designer as a stand-alone here; https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/touchgfxdesigner.html
- Labels:
-
STM32CubeMX
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 8:12 AM
I was able to (eventually) get a STM32CubeMX started project fully working in Atollic TrueSTUDIO for an STM32F746G-DISCO board.
If you are targeting Atollic TrueSTUDIO, below are some useful notes based on what I found:
Web guides of note:
A) Overall guide – except missing specific Atollic True Studio usage. FOLLOW the STM32CubeMX start path of the tree… https://touchgfx.zendesk.com/hc/en-us/articles/360020001492-Getting-Started-with-CubeMX-and-TouchGFX
B) Missing C++ Symbols: https://community.st.com/s/question/0D50X00009bMlNPSA0/convert-cubemx-project-in-atollic-to-c-pane-to-input-symbols-for-c-missing NOTE: I found a better way, - see below ADDING C++ section.
C) TouchGFX – as close to a help file as we get… https://touchgfx.zendesk.com/hc/en-us/categories/200529271-Getting-Started
Steps:
1) Configure your board in SMT32ubeMX, then follow the instructions for adding TouchGFX Middleware under GRAPHICS found on web guide A) – size your display for the real display, not their example. This will start your TouchGXF Designer project as well. For that part, any rough layout is fine – finish the visual/functional design later.
2) Under the “Project Manager�? tab, “Project�? block, set your project name, pick TrueSTUDIO Toolchain/IDE, select a heap & stack size. I picked to copy all used libraries in the “Code Generator�? block – but it didn’t get them all.
3) Generate code in STM32CubeMX – follow the instruction order in web guide A) which creates a TouchGFX project as well.
4) Save your SMT32CubeMX and TouchGFX projects for further use.
Copy the files indicated by web guide A) into the project folders.
5) Start Atollic TrueSTUDIO – note that your Workspace location cannot contain your actual project files!! (This messed me up for a while). In your workspace (I suggest one workspace per project!!), import the project you created with STM32CubeMX. It won’t compile – there’s a lot of work to do yet…
6) Change the project in TrueSTUDIO to a C/C++ project (it’s a pure C project as generated!!). To do so, in TrueSTUDIO select ‘File’ under the main menu. Hover over ‘New’ and on the pop up list, select ‘Convert to a C/C++ Project (Adds C++ Nature)’.
Add the needed include paths to the new C++ compiler settings: Menu ‘Project’ -> ‘Properties’ ->’C/C++ General’->’Paths and Symbols’. 1) If you look at the GNU C++ Language, you will see that it is EMPTY. Use the ‘Export Settings’ to generate an XML file – edit that XML file in Notepad++. Duplicate the section <language name="C Source File"> and name the new one <language name="C++ Source File">. Save the edited version. In TrueSTUDIO, use the ‘Import Settings’ – now the GNU C++ language has the same paths as is needed.
7) Under the ‘Libraries’ tab, if missing, add ‘touchgfx-float-abi-hard’ and ‘touchgfx’ (Note: the file names are libtouchgfx-float-abi-hard.a and libtouchgfx.a but GNU adds the ‘lib’ and the ‘.a’)
8) Under ‘Library Paths’ add Middleware/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc (provided your processor is an m7).
9) Under the ‘C/C++ Build’->’Settings’->’Tool Settings’->’C++ Compiler’->’Optimization’, check the box beside ‘Disable RTTI’
10) Close project properties. In the ‘Project Explorer’, go through the folders and for all ‘template’ files and other IDE types, use a right click menu ‘Resource Configuration’->’Exclude from Build’ (select all configurations) to keep them from being compiled. The same for the whole folders ‘build’ and ‘simulator’ under folder ‘TouchGFX’.
11) This is probably not the proper way to do this step, but it works: Edit file ‘startup_stm32f746xx.s’ (where 746 becomes your exact processor type). Replace the line about ½ way down the file ‘.thumb_set SysTick_Handler,Default_Handler’ with ‘.thumb_set SysTick_Handler,osSystickHandler’. This sets up the proper SysTick interrupt handler – but the expected method is to use a define in an include file – which is hard to follow in a debugger!!
12) The project may compile and debug now. Maybe. Use TouchGFX to design your screens, and TrueSTUDIO to work out the underpinings. Follow web guide C) for linking actions to software.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 9:40 AM
​bbenntett,
Could you please list the versions you used for TouchGFX, TrueStudio and CubeMX?
I am using the latest versions and struggling to setup a starter project as well.
Thank You
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 11:08 AM
I apologize for failing to include revision information! TouchGFX version 4.10, Atollic TrueSTUDIO 9.1.0 Build 20181011-1241 and STM32CubeMX Version 5.0.1 (of V1.0)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 12:41 PM
​Thank for the info.
I've managed to Compile, but when creating the elf file I get the error 'Cannot run program "arm-atollic-eabi-g++": Command line too long" and it is big.
I am running Windows 7, are you under Linux? This is a common error under Eclipse and Windows.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 1:19 PM
I am using Windows 10, and no issues with the extremely long command for linking -
arm-atollic-eabi-g++ -o TouchGFXCube.elf Core\Src\freertos.o Core\Src\main.o Core\Src\stm32f7xx_hal_msp.o Core\Src\stm32f7xx_hal_timebase_tim.o Core\Src\stm32f7xx_it.o Core\Src
[...]
\STM32F746GDISCOTests3\CubeGenTouchGFX\TouchGFXCube\Middlewares\ST\TouchGFX\touchgfx\lib\core\cortex_m7\gcc -L../Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc -Wl,-cref,-u,Reset_Handler -Wl,-Map=TouchGFXCube.map -Wl,--gc-sections -Wl,--defsym=malloc_getpagesize_P=0x1000 -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
(ironically too long to post:* )
This eclipse plug-in might help: https://mcuoneclipse.com/2015/03/29/solving-the-8192-character-command-line-limit-on-windows/
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-18 2:38 PM
Ok, I figured since your referencing the TouchGFX Lib​ that we don't really need to compile most of the framework source. That seemed to improve the cmd line by about 10k.
So...
C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.2.0\ide\jre\bin\java -jar C:\Program Files (x86)\Atollic\TrueSTUDIO for STM32 9.2.0\Tools\arm-atollic-reports.jar sizeinfo list STM32F746-DISCO.elf
Generate build reports...
Print size information
text data bss dec hex filename
1006818 1764 43656 1052238 100e4e STM32F746-DISCO.elf
Print size information done
Generate listing file
Output sent to: STM32F746-DISCO.list
Generate listing file done
Generate build reports done
arm-atollic-eabi-objcopy.exe -O ihex STM32F746-DISCO.elf STM32F746-DISCO.hex
17:29:13 Build Finished (took 1m:52s.725ms)
Progress at least. now to Flash the Target and debug...
BTW, I am using Atollic 9.2.0, and your post has been the most helpful so far.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-19 5:36 AM
@Soren Myllerup MIKKELSEN​ , this information really needs to be a sticky page that can be quickly found. Wasted days in trying to work with a STM32769I-DISCOVERY kit only to realize, this past weekend with thanks to @Martin KJELDSEN​ , that v2.0.0 template is much more refined than template v1.1.0 for this target.
We did find the same Draupner landing page but there is NO mention of the v2.0.0 template use - can that webpage be updated? So the proper "temp fix" would have been to start with this thread and then go to the Draupner page once the IOC project is broken.
Even template v2.0.0 appears to break once CubeMX imports the generated IOC project file and GENERATE CODE is selected inside of CubeMX. Your article on Draupner website is for the most parts, accurate but with assorted typos. After CubeMX breaks the working IOC file, the corrections must be manually applied (as noted on the Draupner landing page).
For future readers, there should be a must read FAQ / sticky page that offers this webpage since this information was available back in December. This info should be quickly available for developers.
The search engine on the ST website is a mess.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-19 2:07 PM
​Success !!
After setting up the ExtFlashSection in the Linker file, ST-LINK to flash, and Setting up the Debugger in atollic. I finally got running and got Hard Fault at x90000000. The USB OTG Host was working , and could store files on the device.
I finally followed the Configuring-STM32F746G-DISCO zendesk article and added the QSPI code from the article.
Now at least the graphics show up on the display. It's too bad it took so long, I was about to give up and go to IAR.
Now I can move forward.
Thanks !!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-02-20 11:58 AM
Hello,
I followed all of your instructions and I got a error with the Libraries...
The compiler is not finding the 'libtouchgfx' and ‘touchgfx-float-abi-hard’ (I did the step 7 carefully and many times in different ways...).
Any idea for this error?
I've tried a lot of guides to generate code from STM32CUBEMX to Atollic with TouchGFX and this tutorial is the most complete and now for me I think is the last error to fix!
Thanks.