‎2023-08-29 6:41 AM - edited ‎2023-08-29 6:45 AM
Hi everyone,
A simple question, I'm using TouchGFX 4.22 with the example "Flex Button Example" for F746G and F7508.
When the program is set to F746 is not possible look all functions of the UART module... See "DinaF746.png"
But if the program is set to F7508 I look and acess all functions of the UART module... See "DinaF7508.png"
What I do need set in TouchGFX or CubeIDE to solve this problem?
Thank you for help.
IGomes
Solved! Go to Solution.
‎2023-08-29 7:18 AM
This is nothing to do with Touch or STM type. Showing this "inteli" is based on setup in IDE for indexing and build...
for example How to turn on auto fill ( auto complete ) in STM3... - STMicroelectronics Community
‎2023-08-29 6:51 AM
You have reply on your png HA_ isnt HAL_
and why you mark this as touchgfx???
‎2023-08-29 7:06 AM - edited ‎2023-08-29 7:12 AM
Hi I attach the correct figure now
my application I'll use F746G TouchGFX and UART integration...
And we really like the TouchGFX
‎2023-08-29 7:18 AM
This is nothing to do with Touch or STM type. Showing this "inteli" is based on setup in IDE for indexing and build...
for example How to turn on auto fill ( auto complete ) in STM3... - STMicroelectronics Community
‎2023-08-29 8:03 AM
Perfect, thanks for the quick response and attention...