2023-10-03 02:54 PM - edited 2023-10-03 03:11 PM
Hello,
I just bought a STM32F746G-DISCO from Mouser (STM32F746G-DISCO STMicroelectronics | Mouser).
After it arrived, the LCD and touch screen were working well. However, after I downloaded the demo project (STM32F746G-DISCO Control LED from GUI v3.0.6) in the TouchGfx 4.22.1, there is not anything displayed. Also I removed the TouchGfx and installed a version, 4.21.3, but there is not any luck.
The board is the blue one. The label on the front is 'STM32F746G-DISCO DK32F746G$CU2', and the label on the back is 'MB1191-F746-C01 / C222103562'.
I found in the previous discussions, the hardware has been changed from version B to version C.
May I know how to generate a WORKIING project with TouchGFX? Thanks.
Solved! Go to Solution.
2023-12-18 04:35 AM
Hello @hbZhao ,
Sorry for the late response,
I tried the board specific demo with a MB1191-F746-C01 (I think it's a bit older than the one you have but shouldn't be any drastic changes), and it works correctly.
Could you please check if you can run other demos (non-board specific ones) on your board? By going in the Demos section and selecting F746 as your Board Setup.
Thank you
2023-12-18 04:35 AM
Hello @hbZhao ,
Sorry for the late response,
I tried the board specific demo with a MB1191-F746-C01 (I think it's a bit older than the one you have but shouldn't be any drastic changes), and it works correctly.
Could you please check if you can run other demos (non-board specific ones) on your board? By going in the Demos section and selecting F746 as your Board Setup.
Thank you
2023-12-18 07:45 AM
Hello Mohammad MORADI,
Thanks for your feedback. This issue has been fixed after I downgraded the development tools.
Best Regards
2023-12-19 12:57 AM
Okay, nice to hear
Good luck
2024-10-14 08:09 PM
@hbZhao
What version did you have to downgrade to? I am currently having this problem.