cancel
Showing results for 
Search instead for 
Did you mean: 

Error when try to flash TouchFx application on my stm32f7508-DK board

MSilv.5
Associate
Flash
        make -f ../gcc/Makefile flash
        Middlewares/ST/touchgfx
        Reading TouchGFX/application.config
        Video Objects:
        Linking TouchGFX/build/bin/target.elf
        Producing additional output formats...
          target.hex   - Combined internal+external hex
          intflash.elf - Internal flash, elf debug
          intflash.hex - Internal flash, hex
              -------------------------------------------------------------------
                               STM32CubeProgrammer v2.10.0                  
              -------------------------------------------------------------------
        
        ST-LINK SN  : 0668FF303931594E43054018
        ST-LINK FW  : V2J39M27
        Board       : STM32F7508-DK
        Voltage     : 3.23V
        SWD freq    : 4000 KHz
        Connect mode: Normal
        Reset mode  : Software reset
        Device ID   : 0x449
        Revision ID : Rev Z
        Device name : STM32F74x/STM32F75x
        Flash size  : 64 KBytes
        Device type : MCU
        Device CPU  : Cortex-M7
        BL Version  : --
        Debug in Low Power mode enabled
        
        
        
        Memory Programming ...
        Opening and parsing file: target.hex
          File          : target.hex
          Size          : 438.90 KB 
          Address       : 0x08000000 
        
        
        Erasing memory corresponding to segment 0:
        Erasing internal memory sector 0
        Erasing memory corresponding to segment 1:
        Erasing external memory sectors [0 3]
        Error: failed to erase memory
        
        
        Error: failed to erase memory
        
        Hard reset is performed
        Done

Above the log.

thank you

1 REPLY 1
MM..1
Chief II

Check in run/debug config right external loader setup for proggrammer.