cancel
Showing results for 
Search instead for 
Did you mean: 

Touchgfx designer 4.22 crashes

awiernie
Senior II

After upgrading from TouchGFX 4.21.3 to Touchfx 4.22.0 the project was converted. If I open the touchgfx project the touchgfx designer crashes:

 

Application: TouchGFXDesigner-4.22.0.exe
CoreCLR Version: 7.0.122.56804
.NET Version: 7.0.1
Description: The process was terminated due to an unhandled exception.
Exception Info: System.IndexOutOfRangeException: Index was outside the bounds of the array.
at TouchGFXDesigner.Communications.NewsManagerViewModel.SwitchCurrentCard(Object state)
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
--- End of stack trace from previous location ---
at System.Threading.ExecutionContext.RunInternal(ExecutionContext executionContext, ContextCallback callback, Object state)
at System.Threading.TimerQueueTimer.Fire(Boolean isThreadPool)
at System.Threading.TimerQueue.FireNextTimers()
at System.Threading.ThreadPoolWorkQueue.Dispatch()
at System.Threading.PortableThreadPool.WorkerThread.WorkerThreadStart()

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Osman SOYKURT
ST Employee

Hello @awiernie 

Could you share with us your 4.21.3 project? We would need it to investigate what's happening here.
(You can share it to me in PM if you prefer).

Osman SOYKURT
ST Software Developer | TouchGFX
awiernie
Senior II

It occures a few seconds after loading (without any user interaction) or after a few minutes with the same windows event log. 

I have sent you a download link for the whole STM32CubeIDE project.