2022-06-23 5:39 AM
Flash
make -f ../gcc/Makefile flash
Middlewares/ST/touchgfx
Reading TouchGFX/application.config
Video Objects:
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
-------------------------------------------------------------------
STM32CubeProgrammer v2.10.0
-------------------------------------------------------------------
ST-LINK SN : 0668FF303931594E43054018
ST-LINK FW : V2J39M27
Board : STM32F7508-DK
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x449
Revision ID : Rev Z
Device name : STM32F74x/STM32F75x
Flash size : 64 KBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : --
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: target.hex
File : target.hex
Size : 438.90 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 3]
Error: failed to erase memory
Error: failed to erase memory
Hard reset is performed
Done
Above the log.
thank you
2022-06-23 8:48 AM
Check in run/debug config right external loader setup for proggrammer.