2021-03-11 4:11 AM
Hello everyone,
I am quite well set up on my project using an STM32F469I-Disco and TouchGFX. Everything is working very well. However, I would like to display data using a dynamic graph. If I choose a mode different from the Scroll mode, everything is updating very well. But when the dynamic graph is in scroll mode it is lagging quite a bit (~1fps) and the touch is almost not responding. How can I improve the performance in my project?
Thank you everyone !
Solved! Go to Solution.
2021-03-14 7:15 PM
Hello NKieg.1,
This problem has already been raised in the community. The development team will have a look at it.
Here is the thread in question (that you are already aware of) : https://community.st.com/s/question/0D53W00000TIAV4SAP/touchgfx-dynamic-graph-widget-scroll-mode-performance-issue
I will close this thread to avoid redundancy. Thank you for your feedback.
/Alexandre
2021-03-12 1:36 AM
Hi,
Do you also face this issue with the simulator or only on the board ? Would you have a project you could share facing this issue ?
/Romain
2021-03-14 7:15 PM
Hello NKieg.1,
This problem has already been raised in the community. The development team will have a look at it.
Here is the thread in question (that you are already aware of) : https://community.st.com/s/question/0D53W00000TIAV4SAP/touchgfx-dynamic-graph-widget-scroll-mode-performance-issue
I will close this thread to avoid redundancy. Thank you for your feedback.
/Alexandre
2021-03-14 11:51 PM
Yes no problem, I will keep checking the other thread then ! Thanks.