2021-11-25 06:40 PM
Assume in dynamic graph, I want to plot value range from 0.0 - 1.0, and I want to setup Y grid and label in between say in step of 0.2. This mean I need the Y grid and Y label on 0, 0.2. 0.4, 0.6, 0.8 and 1.0. Is this doable?
It seems to me TouchGFX Designer Y-label and Y-grid resolution is 1, but I could be wrong.
2021-11-30 09:31 AM
2025-02-10 12:04 PM
Old post, but I stumble into the same problem.
Here is what is needed to display labels every 0.2 steps on the Y axis.
Graph.setGraphRangeY(0.0f, 1.0f);
GraphMajorYAxisLabel.setLabelDecimals(1);
GraphMajorYAxisLabel.setInterval(0.2f);