cancel
Showing results for 
Search instead for 
Did you mean: 

DSI Host Controller with OTM8009A Timeout on Write

Iris-DM
Associate II

I have a custom board with a STM32H747 micro on board, interfacing with a LCD driven by OTM8009A over the MIPI DSI interface. I have taken the driver code from the DISCO eval board which I used to design and build my board. On calling OTM8009A_Init(), the first four write reg calls run fine - entering in command 2 mode and set EXTC to enable address shift function and entering ORISE command 2 and shifting the address to 0x80 - however, every write command after that fails with a timeout. The timeout appears to be generated by the command FIFO being full and not clearing.

Firstly, how likely is this to be down to a hardware error with the board itself?

Secondly, if it is more likely down to the hardware configuration in the micro, what should be the first thing to investigate? I have copied the CubeMX setup from the eval board demo that I had running.

Finally, what's the best way to debug the physical communications between the micro and screen on the DSI lines? What should I be looking for to indicate a hardware error?

 

EDIT:

The specifics of the issue do not change, even if the screen is disconnected! So there must first be a hardware problem to solve.

0 REPLIES 0