2020-08-05 12:05 PM
Hello everyone,
I'm in the community and I started to study the STM32H7 microcontroller familly and the TOUCHGFX. After reading a few post here i discovered that there are some microcontroller the are not suppported by the TOUCHGFX enginne (apparently all the DUAL CORE MCU). If so, I would like to confirme if the STM32H743IIT6 if supported by the TOUCHGFX.
Bruno
Solved! Go to Solution.
2020-09-08 9:33 AM
Hello,
The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.
If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.
/Alexandre
2020-09-08 9:33 AM
Hello,
The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.
If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.
/Alexandre