2023-08-15 8:20 AM - edited 2023-08-15 5:36 PM
I used STM32CubeIDE to create the LCD_DSI_CmdMode_DoubleBuffer for the STM32F769I-DISCOVERY board. It works fine, but I made some modifications to just draw a rectangle:
if 1
BSP_LCD_SetTextColor(LCD_COLOR_RED);
BSP_LCD_FillRect(0, 0, 800, 240);
#else
/* Display example brief */
LCD_BriefDisplay();
/* Copy Buffer 0 into buffer 1, so only image area to be redrawn later */
CopyBuffer((uint32_t *)Buffers[0], (uint32_t *)Buffers[1], 0, 0, 800, 480);
/*Draw first image */
CopyBuffer((uint32_t *)Images[ImageIndex++], (uint32_t *)Buffers[front_buffer], 240, 160, 320, 240);
pend_buffer = 0;
#endif
/* Send Display On DCS Command to display */
HAL_DSI_ShortWrite(&(hdsi_discovery),
0,
DSI_DCS_SHORT_PKT_WRITE_P1,
OTM8009A_CMD_DISPON,
0x00);
/* Refresh the LCD display*/
HAL_DSI_Refresh(&hdsi_discovery);
#if 1
/* Infinite loop */
while (1);
#else
/* Infinite loop */
while (1)
{
if(pend_buffer < 0)
{
/* Prepare back buffer */
CopyBuffer((uint32_t *)Images[ImageIndex++], (uint32_t *)Buffers[1- front_buffer], 240, 160, 320, 240);
pend_buffer = 1- front_buffer;
if(ImageIndex >= 2)
{
ImageIndex = 0;
}
/* Refresh the display */
HAL_DSI_Refresh(&hdsi_discovery);
/* Wait some time before switching to next stage */
HAL_Delay(2000);
}
}
#endif
However the red rectangle is only partially drawn (it's supposed to take up half the screen):
If I put a HAL_Delay before the refresh, it draws the whole rectangle. This suggests the DMA2D isn't finishing the transfer to the framebuffer even though it says it is (HAL_DMA2D_PollForTransfer() is returning in LL_FillBuffer()), but I'm really not sure as I'm pretty new to this stuff.
Thanks in advance.
Solved! Go to Solution.
2023-08-15 7:01 PM
Turns out if I add a delay right after turning on the display, it works fine:
/* Send Display On DCS Command to display */
HAL_DSI_ShortWrite(&(hdsi_discovery),
0,
DSI_DCS_SHORT_PKT_WRITE_P1,
OTM8009A_CMD_DISPON,
0x00);
HAL_Delay(1);
BSP_LCD_SetTextColor(LCD_COLOR_BLUE);
BSP_LCD_FillRect(0, 0, 800, 240);
/* Refresh the LCD display*/
HAL_DSI_Refresh(&hdsi_discovery);
My guess is that there's an issue with the refresh occurring so soon after turning on the display.
2023-08-15 7:01 PM
Turns out if I add a delay right after turning on the display, it works fine:
/* Send Display On DCS Command to display */
HAL_DSI_ShortWrite(&(hdsi_discovery),
0,
DSI_DCS_SHORT_PKT_WRITE_P1,
OTM8009A_CMD_DISPON,
0x00);
HAL_Delay(1);
BSP_LCD_SetTextColor(LCD_COLOR_BLUE);
BSP_LCD_FillRect(0, 0, 800, 240);
/* Refresh the LCD display*/
HAL_DSI_Refresh(&hdsi_discovery);
My guess is that there's an issue with the refresh occurring so soon after turning on the display.