DISPLAY PROGRAMMING CODE AND READ WRITE PROGRAMMING
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-21 2:42 PM
Hi Team
I am using STM32H7B31-DK
I want to use display that is on the board and show my print messages on the screen I see that
i want an application code that helps me to send the print messages data to the LCD on the board
i see that there is nothing like LCD read and write functions similar to UART
Please help me out how to use this code and initialize the display and send my print messages
I see that LTDC that is enabled on my board ia m not sure how to use this and display my messages or any apis
Thank you
Deepak R
- Labels:
-
LCD-LTDC
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-21 11:51 PM
Look in Cube examples for Discovery - like boards with LCD. The BSP drivers for these boards can draw text.
-- pa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-22 1:12 AM
Thing is that the display doesn't work like a UART. The frame buffer is full of pixels, like a bitmap file, text has to be draw from a font table, and a pointer into the display advanced. Once the available space has been exhausted the frame buffer needs to be scrolled up a line to allow a new one to be started/filled.
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
2020-10-22 5:39 AM
I am planning to use an external power supply instead of stlink cable so I am not sure if usart still works to get the logs if I change the pin configuration hence thought of using display to see the text
can you please guide me a way so that I still get the logs but use a different power supply (I.e from a battery device instead of USB ) I hope this works if I use power supply from arduino
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-22 5:40 AM
Can you please share those examples I see that these examples does not have a IOC extension files to enable other features like RTos
I need rtos combined with display example
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-22 5:53 AM
If board has MicroSD card or eMMC one could log data to those.
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
2020-10-22 5:59 AM
Hi clive
yes it has SD card. But what is the procedure to get that working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-22 6:01 AM
Can I get a code of display even if complete screen changes it’s ok I want to make sure system is running and changes are seen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-22 6:06 AM
You'll need to work through the CubeH7 supplied example, applications and demos for the board, and then extract the functionality you need.
Up vote any posts that you find helpful, it shows what's working..