cancel
Showing results for 
Search instead for 
Did you mean: 

Debugging TouchGFX generated project using CubeIDE for STM32F750 board leads to a hardfault

Kasun Dinesh
Associate III

Hi,

I created a project using touchgfx for H750 board. Then I import it to cubeide and started debugging. When i run it, it stopped inside the hardfault.

I am using Touchgfx 4.13 and cubeide 1.3.1. I can debug (step in to different lines) until i start the RTOS task. Once i run the code after that, it stops on hardfault.

Can someone help me out on this?

Thank you

1 REPLY 1
Martin KJELDSEN
Chief III

Hi, when you say "I created a project using touchgfx", do you mean the designer?

/Martin