cancel
Showing results for 
Search instead for 
Did you mean: 

DAC not working with TouchGFX

Riccardo Franceschetto
Associate III

Hi, i'm working on a project where TouchGFX is running, but when i call the DAC via a FreerTOS task, nothing shows up in the output...

Hardware wise everything is ok, tested baremetal and with a single FReertos Task, so TouchGFX or some interrupts might be the problem.

any suggestion?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Not much info here.

Basic debugging steps should be taken. Set up a breakpoint in the relevant code and see if it's getting there. Run the program, then pause and see if processor is stuck somewhere.

Include your chip number so we don't have to guess.

If you feel a post has answered your question, please click "Accept as Solution".