2023-01-15 07:05 AM
TouchGFX 4.21
I have defined a user container: "Selection".
The container contains two buttons: switchToScreenOne and switchToScreenTwo.
I have also defined an interaction for each button that changes the screen.
I have defined two screens: One, Two.
Both screens contain the container "Selection1"
The process works fine.
Question: How can I set the color of the buttons in the containers in the ScreenOneView::setupScreen() function?
I have already tried everything and just can't find the solution.
Solved! Go to Solution.
2023-01-15 07:11 AM
Simply create method in container
2023-01-15 07:11 AM
Simply create method in container
2023-01-15 08:04 AM
THX. That works. But it is still very cumbersome. :-(
2023-01-15 08:09 AM
Why normal C++ objects in class is private = cant manipulate outside class.