2020-07-09 12:51 AM
The compiler throws warnings in touchgfx library files when compiling my project. I would like to know how to solve this. Will it create any issues? I'm using stm32cubeide and gcc-arm-none-eabi-8-2018-q4-major compiler.
2020-07-09 1:15 AM
Please provide a thorough description of your issue before posting =) Now i have to ask you for a log or a printout of those warnings, and you have to write another post, and i have to write another post.
/Martin
2020-07-09 1:25 AM
Hi,
Could you share those warnings? What is your setup?
/Romain
2020-07-09 1:29 AM
Hi @Martin KJELDSEN , @Romain DIELEMAN
Description Resource Path Location Type
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Cell.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/canvas_widget_renderer line 84 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Cell.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/canvas_widget_renderer line 85 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Cell.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/canvas_widget_renderer line 100 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Cell.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/canvas_widget_renderer line 101 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] DragEvent.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/events line 155 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] DragEvent.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/events line 169 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Drawable.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx line 566 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 202 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 216 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 311 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 312 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 357 C/C++ Problem
conversion from 'int' to 'int16_t' {aka 'short int'} may change value [-Wconversion] Types.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/hal line 358 C/C++ Problem
conversion from 'int' to 'uint16_t' {aka 'short unsigned int'} may change value [-Wconversion] Font.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx line 74 C/C++ Problem
conversion from 'int' to 'uint16_t' {aka 'short unsigned int'} may change value [-Wconversion] Font.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx line 88 C/C++ Problem
conversion from 'int' to 'uint16_t' {aka 'short unsigned int'} may change value [-Wconversion] Font.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx line 116 C/C++ Problem
conversion from 'int' to 'uint16_t' {aka 'short unsigned int'} may change value [-Wconversion] Font.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx line 348 C/C++ Problem
conversion from 'int' to 'uint16_t' {aka 'short unsigned int'} may change value [-Wconversion] LCD.hpp /GUI_Lato-Debug@build/[Source directory]/middlewares/touchgfx/framework/include/touchgfx/lcd line 616 C/C++ Problem
2020-07-10 6:01 AM
Hello,
Could you provide the steps you did before compilation (open that software, generated from what, etc.) ? Also what board are you using ? Is it a custom board or a DISCO/EVAL board from ST ?
What kind of GUI are you trying to run ?
/Alexandre
2020-07-11 6:01 AM
follow this guy
https://www.youtube.com/watch?v=o42r4xXOnbo
I do not know which board you are using the problem is that CoubeIDE does not generate all files, you need manually copy and link files/directories
I got with my STM32F469 to a point that CubeIDE compiles without any problems but I still cannnot get the screen to display something. I am missing something simple I cannot find.
you need to study it for a year which is not an opption people would get discouraged or have a good video tutorial and you can have your board running next 30 min
2020-07-15 5:14 AM
Hi,
I'm using custom board with STM32H7 series controller, and designed UI using touchgfx designer. Copied the code generated by the designer to my project. Added all the necessary files to the project and it is running successfully. Only thing is compiler throws above warning in library files.
2020-07-15 5:19 AM
I'm using custom board with STM32H7 series micro controller. Project is running successfully and displaying images. I'm not using CubeIDE for project creation. Designing GUI using touchgfx designer and manually configured all the necessary peripherals, copied the necessary files and libraries from touchgfx generated code, modified linker file. Only issue is compiler throws warning in library files when compiling.
2020-07-15 5:22 AM
Hi,
Im using touchgfx designer for UI design and copied all the necessary files from the designed and included in my project. Project is running without any issues and it is working as expected. Only thing is compiler is throwing above warnings while compiling.