2023-04-17 11:26 PM
Use touchgfx example with stm32f429 discovery Keil with st link usb
When I download it with 2 wire (swd), I get the message cannot load flash programming algorithm. Is there a solution?
(It is the same even if you change the debug option 0x10000000 or 0x20000000. Please help)
2023-04-17 11:32 PM
Can't load it because why?
Can't find it?
Too large to fit in memory?
The wrong one?
Needs more than one for different memory?
Needs Single or Dual bank?