cancel
Showing results for 
Search instead for 
Did you mean: 

cannot launching the TouchGFX DESIGNER 4.19.0

Salar1993
Associate

hello friends
My program does not run! It stays on the initial startup screen.
I have reinstalled the program several times, but it did not fix it.
Can you give me some advice?

2 REPLIES 2
MM..1
Chief III

Maybe try this 

MM1_0-1728739759522.png

 

Imen.D
ST Employee

Hello @Salar1993 ,

Did you try to install the latest release TouchGFX DESIGNER (v 4.24.1)

Is this issue was also faced with latest release ?

Which Windows version do have on your PC?
If possible, share the log file that contains the message and steps when you use the tool, during TouchGFX Designer startup, connection to servers.
The logs of TouchGFX Designer are contained inside C:\Users\username\AppData\Roaming\TouchGFX-<version>\TouchGFXDesigner.log.

 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen