cancel
Showing results for 
Search instead for 
Did you mean: 

Bug Report for Designer assing in multiple textbuffers for wildcard (4.10.0)

brianshankland9
Associate II

I created a custom container in which I placed a scrollwheel.

I added in the item template and selected item template both of which use text with wildcard placements.

The problem arises when I select these text widgets to use a wildcard buffer at which point multiple identically named buffers are defined in the controls base class which cause the compiler to fail.

I have replicated in a small project whch I can zip and email if you say who can deal with this.

1 ACCEPTED SOLUTION

Accepted Solutions
Martin KJELDSEN
Chief III

Hi @brianshankland9​,

This issue was present in 4.10.0 but has been fixed in 4.11.0.

View solution in original post

2 REPLIES 2
Martin KJELDSEN
Chief III

Hi @brianshankland9​,

Please share the project with me. How do you want to do it? Which version of TouchGFX is this?

(Thanks for your report. I'll gladly check to see if you're right)

Best regards,

Martin

Martin KJELDSEN
Chief III

Hi @brianshankland9​,

This issue was present in 4.10.0 but has been fixed in 4.11.0.