cancel
Showing results for 
Search instead for 
Did you mean: 

Artifacts in the simulator and generator. TouchGFX + STM32F407+ILI9488

AFili.1
Associate

Hello everyone!

Faced an interesting problem.

When generating the TouchGFX code, strange artifacts began to appear on the display screen.

At first I decided that the problems were in the display driver. But then I looked through the memory and made sure that the problem was in the generated buffer.

Then, running the simulator in TouchGFX, I found that the problem is displayed there as well

I attach a screenshot of the designer and simulator

0693W00000GWYNHQA5.png 

What could be the problem?

1 REPLY 1
MM..1
Chief III

Know trouble you need set 90 angle images...