cancel
Showing results for 
Search instead for 
Did you mean: 

Adding source files to simulator Makefile in TouchGFXDesigner

JVALL.1
Associate III

Hi,

I am trying to add files from an external library to be build and executed with the TouchGFXDesigner simulator.

Using TouchGFX 4.20 in Windows 10:

In the Makefile under "TouchGFX/simulator/gcc/Makefile" I am adding the following:

ADDITIONAL_SOURCES := ../STM32CubeIDE/library/source
ADDITIONAL_INCLUDE_PATHS := ../STM32CubeIDE/library/include

But when I try to run the simulator I get the following error:

C:/ST/TouchGFX/4.20/env/MinGW/bin/../lib/gcc/i686-w64-mingw32/7.3.0/../../../../i686-w64-mingw32/bin/ld.exe: cannot find ../STM32CubeIDE/library/source: Permission denied

If I add only the "ADDITIONAL_INCLUDE_PATHS" I don't get any error but when I also add the "ADDITIONAL_SOURCES" then is when the error appears.

Not sure how the permission problem can relate to Windows.

0 REPLIES 0