Will the example for mbedtls hardware acceleration in STM32U5 be updated?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-20 12:01 AM
When I use mbedtls on my STM32U585 core board without enabling hardware acceleration, it works fine. However, when I follow the instructions in some posts and copy examples, such as the rsa_alt from SBSFU under STM32U5Cube, many errors appear, and it seems difficult to fix. I noticed that the mbedtls in STM32CubeU5 seems to be several versions behind. I also tried using H5 for porting, but the result is still not satisfactory. Will there be new hardware acceleration examples for STM32U585 using STM32-MW-MBEDTLS? Thank you."
- Labels:
-
Bug-report
-
Cryptography
-
SBSFU
-
STM32 Security
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-23 3:04 PM
Hi @linglitel,
I'm checking internally if there are plans to update the mbedTLS version and provide new hardware acceleration examples for STM32U5.
I guess you know the following link: GitHub - STMicroelectronics/stm32-mw-mbedtls: Mbed TLS is an open source, portable, easy to use, readable and flexible TLS library, and reference implementation of the PSA Cryptography API.
The stm32-mw-mbedtls release is v3.6.2_20250204 versus 2.8 release in STM32Cube_FW_U5_V1.7.0.
In the mean time, can you check the last release if it is helpful ?
Best Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-24 3:15 AM
Thank you for your reply.
I have already used this library, and it performs very fast. However, I am not able to determine whether hardware acceleration is actually being used. Due to the large version gap between STM32Cube_FW_U5_V1.7.0 and stm32-mw-mbedtls, I cannot use the examples from STM32Cube_FW_U5_V1.7.0 to enable hardware acceleration properly.
The STM32U585 has powerful security features, and I believe hardware acceleration is essential to fully utilize its capabilities.
At the same time, I found that both stm32-mw-mbedtls and X-CUBE-CRYPTOLIB consistently produce incorrect SHA256 results when TrustZone is enabled. I have already opened a support ticket, but they advised me to seek help through the community.
Could you please help with this issue?