cancel
Showing results for 
Search instead for 
Did you mean: 

SBSFU | B-L4S5I-IOT01A | Build error | Missing function definitions

Jakub Standarski
Associate III

Hello all,

I'm trying to build B-L4S5I-IOT01A, 2 Images KMS project and I'm encountering the build issue related with missing function definition for KMS_LL_Finalize(). Build fails during linkage phase.

JakubStandarski_0-1706106424035.png

Is that issue related with the wrong version of KMS package provided with SBSFU 2.6.2?

 

PS. Same issue applies for B-L475E-IOT01A project.

4 REPLIES 4
Jocelyn RICARD
ST Employee

Hello Jakub,

yes, this is that issue.

Just get KMS middleware from SBSFU 2.6.1 and copy it in SBSFU 2.6.2 it will solve the issue

Best regards

Jocelyn

 

Bubbles
ST Employee

Hello @Jakub Standarski,

what tool did you use to build the project? There is apparently some sort of regression when using newer tool. I encountered same problem using EWARM 9.40, while in EWARM 9.30 it built correctly.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STM32CubeIDE 1.12.1.

I've checked code and definition for the function mentioned above doesn't exist.
I will try KMS version provided by SBSFU 2.6.1 as mentioned by @Jocelyn RICARD .

Thank you for you help!

Bubbles
ST Employee

Hi @Jakub Standarski ,

problem is reported fixed in version 2.7.0.

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.