2021-06-09 1:36 AM
Hi,
I followed document "readme.txt" in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" to family with TFM, it work fine.
My question:
1: "press reset button or restart the board power" will lock the board.
Please tell me what code in the "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" cause the board locked, and list the code for me.
2:"Remove JP2 jumper on STM32L562E-DK board, then put it back in place" can unlock the board, but I can't unlock the board via restarting the board power. please explain more detailly for me, or show me what code is used to unlock the board in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM".
Thanks,
QiZhang
2021-06-09 9:34 AM
Hi @zqizh.1 ,
If you would like to understand more how TFM application is working, you need to study the user manual UM2671 Getting started with STM32CubeL5 TFM application.
You will find there a more detailed explanation than the readme. This document describes also the firmware architecture of this application that can help you to identify the exact code executed while doing some actions.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-06-09 6:01 PM
Hi Amel,
I've read the user manual UM2671 and review the TFM application code, but I can't get answer from their.
Please review my question and advise.
Thanks ,
QiZhang