2024-02-07 10:18 AM
Hello,
I'm trying to run the X-CUBE-IOTA1 v3.0 on the B-U585I-IOT02A board, but after following the tutorial in UM2606 I get the following error when trying to send L2Sec Stream:
What can be the reason of the pairing_stsafe result failing, please?
Best regards,
@Jocelyn RICARD @Benjamin BARATTE
Solved! Go to Solution.
2024-02-08 07:26 AM
Hi @SedCore,
I think this issue is related the change of the STSAFE-A power management on B-U585-IOT2A board.
The error reported (1) is STSAFEA_COMMUNICATION_ERROR which generally occurs on the first STSAFE-A commands when the STSAFE-A is not responding on the I2C.
According to the User Manual of the B-U585-IOT2A board, the PF11 pin shall be 0 to enable the STSAFE-A.
In the X-CUBE-IOTA v3.0.0 x-cube-iota1/Projects/B-U585I-IOT02A/Applications/IOTA-Client/NetXDuo/App/STSAFE/stsafea_service_interface.c
in the HW_IO_Init, you have this line which set the PF11 to 1 :
HAL_GPIO_WritePin(STSAFEA_VREG_GPIO_PORT, STSAFEA_VREG_PIN, GPIO_PIN_SET);
Therefore, this disabled the STSAFE-A.
if you replace the line by HAL_GPIO_WritePin(STSAFEA_VREG_GPIO_PORT, STSAFEA_VREG_PIN, GPIO_PIN_RESET);
It should enable the STSAFE-A and you should be able to run the test code.
Best Regards,
Benjamin
2024-02-08 07:26 AM
Hi @SedCore,
I think this issue is related the change of the STSAFE-A power management on B-U585-IOT2A board.
The error reported (1) is STSAFEA_COMMUNICATION_ERROR which generally occurs on the first STSAFE-A commands when the STSAFE-A is not responding on the I2C.
According to the User Manual of the B-U585-IOT2A board, the PF11 pin shall be 0 to enable the STSAFE-A.
In the X-CUBE-IOTA v3.0.0 x-cube-iota1/Projects/B-U585I-IOT02A/Applications/IOTA-Client/NetXDuo/App/STSAFE/stsafea_service_interface.c
in the HW_IO_Init, you have this line which set the PF11 to 1 :
HAL_GPIO_WritePin(STSAFEA_VREG_GPIO_PORT, STSAFEA_VREG_PIN, GPIO_PIN_SET);
Therefore, this disabled the STSAFE-A.
if you replace the line by HAL_GPIO_WritePin(STSAFEA_VREG_GPIO_PORT, STSAFEA_VREG_PIN, GPIO_PIN_RESET);
It should enable the STSAFE-A and you should be able to run the test code.
Best Regards,
Benjamin
2024-02-08 09:01 AM - edited 2024-02-09 01:53 AM
Thanks for your advice, now the encryption using STSAFE is working well. 👍👍
But unfortunately, the message is not being sent, due to a DNS error when trying to connect to the Tangle network at this address: https://api.lb-0.h.chrysalis-devnet.iota.cafe
There is no public network running the Chrysalis protocol anymore, so the X-CUBE-IOTA1 package should be updated.
2024-02-14 06:46 AM
Hello @SedCore
the X-CUBE-IOTA1 package is going to be archived and will not be updated.
Kind regards
Andrea
2024-03-19 10:57 PM
2024-03-19 11:07 PM
2024-03-21 03:13 AM - edited 2024-03-21 03:14 AM
Hello, Chrysalis has been archived by the IOTA Foundation. The Tangle is now in the Stardust stage.
2024-03-21 05:58 AM - edited 2024-03-21 05:59 AM
2024-03-25 04:58 AM - edited 2024-03-25 04:59 AM
X-CUBE-IOTA package seems to rely on the IOTA C library, which is now archived: https://github.com/iotaledger/iota.c
So, there is no longer a working IOTA API in C language. I'm not sure the existing archived C library can work with Stardust. Maybe this could help: https://github.com/iotaledger/iota-sdk-native-bindings
BR.
2024-03-26 05:35 PM
Thank you for your reply.
So you mean Now X-CUBE-IOTA doesn't work properly...
I will try to modify this application code to fit the stardust protocol...
But I am not sure it is possible.
Thank you so much!