Hi @tobbymathew, For Secure Boot on STM32, please reference to the X-CUBE-SBSFU package.You will find in the UM2262, the STSAFE-A is used only with STM32L4.Regarding the firmware signing with OpenSSL, this will depends on the FW image you need to sig...
Hi @y_yamamoto, The Wrap/Unwrap use case is encrypting a data with a key known only by the STSAFE-A110.In order to perform this operation in a secure way, the I2C link shall be protected.Therefore, the Wrap command mandate to encrypt the data with th...
Hi @Kombo , Thanks for your interest to ST Solution Regarding the STSAFE-A110 solution for Qi 1.3 you need to have a custom personalization.Even with test sample, they are not compatible for official Qi device. This is only for testing.To be compatib...
Hi @y_yamamoto , Actually, the I2C parameters can be changed by personalization.On evaluation part (STSAFA110xxSPL02/3), you can change the I2C address as well.You need to use the StSafeA_PutAttribute() command with InAttributeTag to STSAFEA_TAG_I2C_...
Hi @LMaarsen,Thanks Bert for your interest in STSAFE-TPM product.The I2C address is defined by TCG within the PTP specification and yes this is 0x2E on 7bits.Best Regards,Benjamin