cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying STM32CubeExpansion_SBSFU_V2.4.0 with 2 Active images and 2 Download areas and assigned the LOcation in mapping_fwimg.icf. Code is building but i am getting error = "[FWIMG] Header of SLOT_ACTIVE_2 is not under the firewall protection"

DMira.11
Associate II

0693W00000ANle9QAD.pngPlease guide me how to add SLOT_ACTIVE_2 to firewall protection.

14 REPLIES 14
DMira.11
Associate II

Can any body help with this??

Ons KOOLI
Senior III

Hi @DMira.1​ ,

Can you please provide more details about the claim:

  • board name
  • project directory
  • Steps you followed to run the project
  • IDE used to run the project

Best Regards,

Ons.

Hi,

Board: Nucleo L476RG

Project directory : ​STM32CubeExpansion_SBSFU_V2.4.0

Ide : stm32 Workbench​

Steps : ​https://www.st.com/resource/en/user_manual/dm00414687-getting-started-with-the-xcubesbsfu-stm32cube-expansion-package-stmicroelectronics.pdf

https://www.st.com/resource/en/application_note/dm00414677-integration-guide-for-the-xcubesbsfu-stm32cube-expansion-package-stmicroelectronics.pdf

@Ons KOOLI​  anything else required?

DMira.11
Associate II

I am in search of solution... Please help..​

Hi @DMira.1​ ,

Sorry for the delay, we were celebrating Aid.

Can you specify which project exactly did you run.

Best Regards,

Ons.

0693W00000AOdXMQA1.pngThere is only one project on L476RG in​ STM32CubeExpansion_SBSFU. It is working with out any issue. But I added 2 active and 2 download slots by modifying Macros SFU_NB_MAX_ACTIVE_IMAGE and SFU_NB_MAX_DWL_AREA. And even i added memory locations in mapping_fwimg.icf. Please refer the image attached. I am getting error SLOT_ACTIVE_2 is not under firewall protection.

Hi @DMira.1​ ,

For me, I found 3 different projects which are :

  • 2_Images_SBSFU
  • 2_Images_SECoreBin
  • 2_Images_UserApp

0693W00000AOe9BQAT.pngBest Regards,

Ons.

All 3 projects we need to add, That is interdependent. Please check Readme for compilation order. And follow https://www.st.com/resource/en/application_note/dm00414677-integration-guide-for-the-xcubesbsfu-stm32cube-expansion-package-stmicroelectronics.pdf