2020-04-17 2:42 AM
Hi support team,
i am testing the sbsfu code in P-NUCLEO-WB55 but i missed out to disable security ips SECBOOT_DISABLE_SECURITY_IPS and flash into the board it set RDP level to 1 also set SFU_WRP_PROTECT_ENABLE, SFU_TAMPER_PROTECT_ENABLE,SFU_DAP_PROTECT_ENABLE,SFU_MPU_PROTECT_ENABLE... .
now i want to remove this code and flash other application but i can not debug or run as application via IDE(AC6 or cubeide) it through error: write protection detected check RDP and WRP protection options.
Please help me out to resolve above issue.
I have change RDP from 1(BB) to 0(AA) but issue is not resolve.
Thanks,
Arjun
2020-04-17 2:59 AM
Per RM0433 and UM2262 and others...
An RDP L0 regression from L1 performs a mass-erase.
So you have to connect a ST-LINK or similar, change the RDP to level 0 (which does the mass-erase) and disable the WRPs.
This leaves user flash empty.
Then you have to re-load the combined SBSFU and app, or just the SBSFU and use it to re-load the app.
2020-04-17 3:11 AM
Hi @alister
Thanks for quick response i am using stcubeprogrammer for change RDP level, it change successfully from 1 to 0 but i can't find how to disable WRPs
please find attached image
Thanks,
Arjun
2020-04-17 3:25 AM
Hi @alister
Thanks for your support resolve the issue by changing WRP1A_START and WRP1A_END (WRPxy_START > WRPxy_END = No WRP or unprotected, as mentioned in RM0434 ).
Thanks,
Arjun
2020-04-17 4:09 AM
STM32CubeProgrammer isn't intuitive. You'll have to check RM0434 and try to correlate its description of WRP with this GUI.
Alternatively, if you have an older tool called "STM32 ST-LINK Utility", that was pretty easy to understand.
2022-12-22 2:45 AM
Hello Everyone, I'm in exactly the same situation.
I've changed RDP and WRPxy_START, WRPxy_END
Please find the values in the below log.
./STM32_Programmer_CLI -c port=swd -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.12.0
-------------------------------------------------------------------
ST-LINK SN : 0671FF313736504157192620
ST-LINK FW : V2J40M27
Board : NUCLEO-G070RB
Voltage : 3.22V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x460
Revision ID : Rev B
Device name : STM32G07x/STM32G08x
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xB2
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 112 Bytes
[==================================================] 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_EN : 0x0 (Configurable brown out reset disabled, power-on reset defined by POR/PDR levels)
BORR_LEV : 0x0 (BOR rising level 1 with threshold around 2.1 V)
BORF_LEV : 0x0 (BOR falling level 1 with threshold around 2.0 V)
User Configuration:
nRST_STOP : 0x1 (No reset generated when entering Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering Standby mode)
nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode)
IWDG_SW : 0x1 (Software independant watchdog)
IWDG_STOP : 0x1 (IWDG counter active in stop mode)
IWDG_STDBY : 0x1 (IWDG counter active in standby mode)
WWDG_SW : 0x1 (Software window watchdog)
RAM_PARITY_CHECK: 0x1 (SRAM parity check disable)
nBOOT_SEL : 0x1 (BOOT0 signal is defined by nBOOT0 option bit)
nBOOT1 : 0x1 (Boot from Flash if BOOT0 = 0, otherwise system memory)
nBOOT0 : 0x1 (nBOOT0=1)
NRST_MODE : 0x3 (Bidirectional reset: NRST pin configured in reset input/output mode (legacy mode))
IRHEN : 0x1 (Internal resets drives NRST pin low until it is seen as low level)
PCROP Protection:
PCROP1A_STRT : 0xFF (0x801FE00)
PCROP1A_END : 0x0 (0x8000200)
PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
PCROP1B_STRT : 0xFF (0x801FE00)
PCROP1B_END : 0x0 (0x8000200)
Write Protection:
WRP1A_STRT : 0x0 (0x8000000)
WRP1A_END : 0x0 (0x8000000)
WRP1B_STRT : 0x3F (0x801F800)
WRP1B_END : 0x0 (0x8000000)
FLASH security:
BOOT_LOCK : 0x0 (Boot based on the pad/option bit configuration)
SEC_SIZE : 0x20 (0x8010000)
Let me know how to resolve this.