cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_CRYPEx_AES() maximum number of output bytes?

dsorber
Associate II

I am using an STM32L4S9ZIJX part and attempting to encrypt a 256KB buffer (actually 262,144 - 16 = 262,128 bytes) using AES256 CTR mode in polling mode.

I created a wrapper function to perform the encryption:

 

int encrypt_CTR_mode(uint8_t* key, uint8_t* IV, uint8_t* plaintext, uint32_t pt_length,
                     uint8_t* ciphertext)
{
    // Deinit old parameters
    if (HAL_CRYP_DeInit(&hcryp) != HAL_OK)
    {
        LOG(error, "ERROR: HAL_CRYP_DeInit() failed\n");
        return -1;
    }

    // Setup new params
    hcryp.Init.DataType = CRYP_DATATYPE_32B;
    hcryp.Init.KeySize = CRYP_KEYSIZE_256B;
    hcryp.Init.OperatingMode = CRYP_ALGOMODE_ENCRYPT;
    hcryp.Init.ChainingMode = CRYP_CHAINMODE_AES_CTR;
    hcryp.Init.KeyWriteFlag = CRYP_KEY_WRITE_ENABLE;
    hcryp.Init.pKey = key;
    hcryp.Init.pInitVect = IV;

    // Init new parameters
    if (HAL_CRYP_Init(&hcryp) != HAL_OK)
    {
        LOG(error, "ERROR: HAL_CRYP_Init() failed\n");
        return -1;
    }

    // Encrypt plaintext
    HAL_StatusTypeDef rc;
    rc = HAL_CRYPEx_AES(&hcryp, plaintext, pt_length, ciphertext, 5000);
    if (rc != HAL_OK)
    {
        LOG(error, "ERROR: HAL_CRYPEx_AES() -- %d\n", rc);
        return -1;
    }

    return 0;
}

 

 

The function returns successfully but I only get 65,520 (0xFFF0) output bytes even though I'm passing in 262,128 to HAL_CRYPEx_AES().  Is there some limitation for the maximum output length of HAL_CRYPEx_AES()?  I can't find any such limitation documented.

 

 

2 REPLIES 2
dsorber
Associate II

Whoops... I see my problem: HAL_CRYPEx_AES() size parameter is a uint16_t.

Thankfully the source is exposed, and deeper hcryp->CrypInCount is uint32_t

You could perhaps also decompose the data into blocks

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..