cancel
Showing results for 
Search instead for 
Did you mean: 

Error occured while provisioning '.obj files' on STM32H573-DK

Choppa
Associate II

hello 

 

I'm using a STM32H573-DK board for engineering samples. 
so. I'm run a example this link but provisioning.bat files does not run at 'Step 3 : Provisioning'

How to fix this problem?

 

provnn_step3.PNG

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

This is a material switch on your board, bottom left not far from RESET. Thre is a serigraphy : BOOT0

View solution in original post

6 REPLIES 6
Choppa
Associate II

attach obkey_programming.log file contents


C:\Users\user\STM32Cube\Repository\STM32Cube_FW_H5_V1.1.1\Projects\STM32H573I-DK\ROT_Provisioning\OEMiROT>call ../env.bat
Configure OBKeys HDPL1-DA config area
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Device name : STM32H5xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xFF
SFSP Version: v0.0.0
Debug in Low Power mode enabled


Hard reset is performed
-------------------------------------------------------------------
STM32CubeProgrammer v2.15.0
-------------------------------------------------------------------

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Device name : STM32H5xx
Flash size : 2 MBytes (default)
Device type : MCU
Device CPU : Cortex-M33
BL Version : 0xFF
SFSP Version: v0.0.0
Debug in Low Power mode enabled

ST-LINK SN : 000600164D46501220383832
ST-LINK FW : V3J13M4
Board : STM32H573I-DK
Voltage : 3.28V
SWD freq : 8000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x484
Revision ID : Rev A
Secure Data Provisioning Start. OBK Input file : ../DA/Binary/DA_Config.obk
Error: Execution of RSS CMD fail with timeout
Error: call_RSSLIB_SetOBKey Failed
лллллллллллллллллллллллллллллллллллллллллллллллллл 100%Error:
OBKey Provisioning failed

 

Frantz LEFRERE
ST Employee

Hello,

insure to change SW has indicate in the trace and then it should works

Br,

Frantz 

Hello LEFRERE.


how to change SW?
Can i see trace and working SW, if i change SW?

 

 

 

 

This is a material switch on your board, bottom left not far from RESET. Thre is a serigraphy : BOOT0

Yes, my board SW1 already set to FLASH (0)

Sorry solved problems, first SW1 set a position 0 and next set 1 finaly set 0.
These processes have not been performed.