2022-04-07 5:01 AM
I've found an inconsistency between different reference manuals of STM32 embedding the CRYP peripheral, about the management of IVs in GCM mode:
The HAL seems to implement the second solution.
Could you confirm ?
Best regards
2022-04-13 12:58 AM
Helllo @Gpeti ,
looking in the STM32H7 Cryp example for GCM, it seems you are right!
uint32_t InitVector[4] = {0xcafebabe,0xfacedbad,0xdecaf888 , 0x00000002};
hcryp.Init.pInitVect = InitVector;
/* Set the initialization vector and the counter : Initial Counter Block (ICB)*/
hcryp->Instance->IV0LR = *(uint32_t *)(hcryp->Init.pInitVect);
hcryp->Instance->IV0RR = *(uint32_t *)(hcryp->Init.pInitVect + 1);
hcryp->Instance->IV1LR = *(uint32_t *)(hcryp->Init.pInitVect + 2);
hcryp->Instance->IV1RR = *(uint32_t *)(hcryp->Init.pInitVect + 3);
I will raise the point internally
Thank you raising the point
Best regards
Jocelyn
2023-02-20 6:19 AM
Hello,
I've just had a look to the new revision of STM32H753 ref manual and this point has not been adressed. A bit disappointing...