2025-07-31 10:58 AM
Hi everyone,
I tried Secure Firmware Install (SFI) with the Nucleo-H563ZI. The process failed, however my device is still accessible.
By connecting to the device via Hot plug and Access port 1 I am able to see that the device is in "Provisioning" state.
The option bytes are as follows:
{
"deviceId" : 1156,
"bitNameToValue" : {
"PRODUCT_STATE" : 23,
"BOR_LEV" : 0,
"BORH_EN" : 0,
"IO_VDD_HSLV" : 0,
"IO_VDDIO2_HSLV" : 0,
"IWDG_STOP" : 1,
"IWDG_STDBY" : 1,
"BOOT_UBE" : 195,
"SWAP_BANK" : 0,
"IWDG_SW" : 1,
"NRST_STOP" : 1,
"NRST_STDBY" : 1,
"TZEN" : 180,
"SRAM2_ECC" : 1,
"SRAM3_ECC" : 1,
"BKPRAM_ECC" : 1,
"SRAM2_RST" : 1,
"SRAM1_3_RST" : 1,
"NSBOOTADD" : 524288,
"NSBOOT_LOCK" : 195,
"SECBOOT_LOCK" : 0,
"SECBOOTADD" : 0,
"SECWM1_STRT" : 0,
"SECWM1_END" : 127,
"WRPSGn1" : -1,
"SECWM2_STRT" : 0,
"SECWM2_END" : 127,
"WRPSGn2" : -1,
"LOCKBL" : 0,
"EDATA1_EN" : 0,
"EDATA1_STRT" : 0,
"EDATA2_EN" : 0,
"EDATA2_STRT" : 0,
"HDP1_STRT" : 1,
"HDP1_END" : 0,
"HDP2_STRT" : 1,
"HDP2_END" : 0
}
}I want to go back to "Open" state. While setting up the SFI-Image I introduced a password authentication, not a certificate.
After the failed SFI-installation process I encountered that the device however had TrustZone enabled, which did not align with the password authentication. So I changed TZEN to 0xC3 instead of 0xB4. After that I performed a debug authentication with my password.bin - without success.
19:22:18 : Start Debug Authentication Sequence
19:22:18 : SDMOpen : 624 : open : SDM API v1.0
19:22:18 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:22:18 : open_comms : 513 : open : Asserting target reset
19:22:18 : open_comms : 517 : open : Writing magic number
19:22:18 : open_comms : 537 : open : De-asserting target reset
19:22:18 : open_comms : 584 : open : Communication with the target established successfully
19:22:18 : discovery: target ID.......................:0x484
19:22:18 : discovery: SoC ID..........................:0x00000000_31393834_32335111_0051003D
19:22:18 : discovery: SDA version.....................:2.4.0
19:22:18 : discovery: Vendor ID.......................:STMicroelectronics
19:22:18 : discovery: PSA lifecycle...................:ST_LIFECYCLE_PROVISIONING
19:22:18 : discovery: PSA auth version................:1.0
19:22:18 : discovery: ST HDPL1 status.................:0xfffffffe
19:22:18 : discovery: ST HDPL2 status.................:0xfffffffe
19:22:18 : discovery: ST HDPL3 status.................:0xfffffffe
19:22:18 : discovery: Token Formats...................:0x200
19:22:18 : discovery: Certificate Formats.............:0x201
19:22:18 : discovery: cryptosystems...................:ST Password
19:22:18 : discovery: ST provisioning integrity status:0xf5f5f5f5
19:22:18 : discovery: permission if authorized...........:Full Regression
19:22:35 : UR connection mode is defined with the HWrst reset mode
19:22:35 : Start Debug Authentication Sequence
19:22:35 : SDMOpen : 624 : open : SDM API v1.0
19:22:35 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:22:35 : open_comms : 513 : open : Asserting target reset
19:22:35 : open_comms : 517 : open : Writing magic number
19:22:35 : open_comms : 537 : open : De-asserting target reset
19:22:35 : open_comms : 584 : open : Communication with the target established successfully
19:22:35 : [00%] discovery command
19:22:35 : [10%] sending discovery command
19:22:35 : [20%] receiving discovery
19:22:35 : [40%] loading credentials
19:22:35 : [50%] sending challenge request
19:22:35 : [60%] receiving challenge
19:22:35 : Error: Debug Authentication Failed
19:22:35 : Disconnected from device.
Afterwards I tried provisioning a new .obk file successfully:
19:24:45 : ST-LINK SN : 001C00303433510D37363934
19:24:45 : ST-LINK FW : V3J10M3
19:24:45 : Board : NUCLEO-H563ZI
19:24:45 : Voltage : 3.27V
19:24:45 : SWD freq : 8000 KHz
19:24:45 : Connect mode: Hot Plug
19:24:45 : Reset mode : Core reset
19:24:45 : Device ID : 0x484
19:24:45 : Revision ID : Rev X
19:24:45 : Secure Data Provisioning Start. OBK Input file : C:\...\STM32H523-H56x_ConfigWithPassword.obk
19:24:45 : OBKey Provisioned successfully C:\Users\...\STM32H523-H56x_ConfigWithPassword.obk Then I disconnected, power-on reset and again same error:
19:26:47 : Start Debug Authentication Sequence
19:26:47 : SDMOpen : 624 : open : SDM API v1.0
19:26:47 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:26:47 : open_comms : 513 : open : Asserting target reset
19:26:47 : open_comms : 517 : open : Writing magic number
19:26:47 : open_comms : 537 : open : De-asserting target reset
19:26:47 : open_comms : 584 : open : Communication with the target established successfully
19:26:47 : discovery: target ID.......................:0x484
19:26:47 : discovery: SoC ID..........................:0x00000000_31393834_32335111_0051003D
19:26:47 : discovery: SDA version.....................:2.4.0
19:26:47 : discovery: Vendor ID.......................:STMicroelectronics
19:26:47 : discovery: PSA lifecycle...................:ST_LIFECYCLE_PROVISIONING
19:26:47 : discovery: PSA auth version................:1.0
19:26:47 : discovery: ST HDPL1 status.................:0xfffffffe
19:26:47 : discovery: ST HDPL2 status.................:0xfffffffe
19:26:47 : discovery: ST HDPL3 status.................:0xfffffffe
19:26:47 : discovery: Token Formats...................:0x200
19:26:47 : discovery: Certificate Formats.............:0x201
19:26:47 : discovery: cryptosystems...................:ST Password
19:26:47 : discovery: ST provisioning integrity status:0xf5f5f5f5
19:26:47 : discovery: permission if authorized...........:Full Regression
19:27:01 : UR connection mode is defined with the HWrst reset mode
19:27:01 : Start Debug Authentication Sequence
19:27:01 : SDMOpen : 624 : open : SDM API v1.0
19:27:01 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:27:01 : open_comms : 513 : open : Asserting target reset
19:27:01 : open_comms : 517 : open : Writing magic number
19:27:01 : open_comms : 537 : open : De-asserting target reset
19:27:01 : open_comms : 584 : open : Communication with the target established successfully
19:27:01 : [00%] discovery command
19:27:01 : [10%] sending discovery command
19:27:01 : [20%] receiving discovery
19:27:01 : [40%] loading credentials
19:27:01 : [50%] sending challenge request
19:27:01 : [60%] receiving challenge
19:27:01 : Error: Debug Authentication Failed
19:27:01 : Disconnected from device.Then I changed back to TrustZone enabled and provisioned with certificates:
19:51:46 : Secure Data Provisioning Start. OBK Input file : C:\workspace\STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Binary\DA_Config.obk
19:51:46 : OBKey Provisioned successfully C:\workspace\STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Binary\DA_Config.obk
19:52:04 : Disconnected from device.And tried regression via Debug Authentication:
19:52:24 : Start Debug Authentication Sequence
19:52:24 : SDMOpen : 624 : open : SDM API v1.0
19:52:24 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:52:24 : open_comms : 513 : open : Asserting target reset
19:52:24 : open_comms : 517 : open : Writing magic number
19:52:24 : open_comms : 537 : open : De-asserting target reset
19:52:24 : open_comms : 584 : open : Communication with the target established successfully
19:52:24 : discovery: target ID.......................:0x484
19:52:24 : discovery: SoC ID..........................:0x00000000_31393834_32335111_0051003D
19:52:24 : discovery: SDA version.....................:2.4.0
19:52:24 : discovery: Vendor ID.......................:STMicroelectronics
19:52:24 : discovery: PSA lifecycle...................:ST_LIFECYCLE_PROVISIONING
19:52:24 : discovery: PSA auth version................:1.0
19:52:24 : discovery: ST HDPL1 status.................:0xfffffffe
19:52:24 : discovery: ST HDPL2 status.................:0xfffffffe
19:52:24 : discovery: ST HDPL3 status.................:0xfffffffe
19:52:24 : discovery: Token Formats...................:0x200
19:52:24 : discovery: Certificate Formats.............:0x201
19:52:24 : discovery: cryptosystems...................:Ecdsa-P256 SHA256
19:52:24 : discovery: ST provisioning integrity status:0xf5f5f5f5
19:52:24 : discovery: permission if authorized...........:Full Regression
19:52:24 : discovery: permission if authorized...........:To TZ Regression
19:52:24 : discovery: permission if authorized...........:Level 3 Intrusive Debug
19:52:24 : discovery: permission if authorized...........:Level 2 Intrusive Debug
19:52:24 : discovery: permission if authorized...........:Level 1 Intrusive Debug
19:52:24 : discovery: permission if authorized...........:Level 3 Intrusive Non Secure Debug
19:52:24 : discovery: permission if authorized...........:Level 2 Intrusive Non Secure Debug
19:52:24 : discovery: permission if authorized...........:Level 1 Intrusive Non Secure Debug
19:53:14 : Start Debug Authentication Sequence
19:53:14 : SDMOpen : 624 : open : SDM API v1.0
19:53:14 : SDMOpen : 625 : open : SDM Library version v1.2.0
19:53:14 : open_comms : 513 : open : Asserting target reset
19:53:14 : open_comms : 517 : open : Writing magic number
19:53:14 : open_comms : 537 : open : De-asserting target reset
19:53:14 : open_comms : 584 : open : Communication with the target established successfully
19:53:14 : [00%] discovery command
19:53:14 : [10%] sending discovery command
19:53:14 : [20%] receiving discovery
19:53:14 : [40%] loading credentials
19:53:14 : [50%] sending challenge request
19:53:14 : [60%] receiving challenge
19:53:14 : Error: Debug Authentication FailedThe integrity status is definetley wrong according to:
• ST provisioning integrity: indicates if integrity of provisioned DA data is correct (0xeaeaeaea) or wrong
(0xf5f5f5f5).
Question:
Is there a way to fix the integrity status 0xf5f5f5f5 and hence perform a full regression?
Best regards
2025-07-31 3:09 PM
Hi @jho ,
it looks like you don't use last version of STM32CubeProgrammer but I doubt this could be the issue.
The fact that you get this integrity status to 0xf5f5f5f5 after provisioning the DA obk, probably means that you have provided an obk with encryption flag.
The obk is valid for provisioning but is invalid as H563 does not have crypto available.
Could you please check this point ?
Best regards
Jocelyn
2025-07-31 10:50 PM
Hi Jocelyn,
I've explicitly selected the DA for the H563 from
STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Binary\DA_Config.obk
Is that correct?
Best regards,
jho
2025-08-01 12:56 AM
Hi jho,
my point was to check that this DA_Config.obk or DA_ConfigWithPassword.obk were correct, in case they have been regenerated.
Now if they are correct, could you please try with latest version of STM32CubeProgrammer.
One last point is regarding your OB setup.
You have BOOT_UBE=0xC3 and TZEN=0xB4 this is configuration to enable STiROT.
But you have BOOT_LOCK and SECBOOT_ADDR that are set to 0 which is not normal or related to the programmer version you have.
Could you check setting BOOT_UBE=0xB4 and try again
Best regards
Jocelyn
2025-08-01 4:02 AM
1. I regenerated a valid DA_Config.obk, completed the provisioning, and reran the regression - but the integrity status is still incorrect.
2. The attempt to change BOOT_UBE to 0xB4 raised an error:
12:45:56 : OPTION BYTE PROGRAMMING VERIFICATION:
12:45:56 : Error: Expected value for Option Byte "BOOT_UBE": 0xB4, found: 0xC3
12:45:56 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCHSimilarly, attempts to change other option bytes such as SECBOOT_LOCK to 0xC3, SECWM1,2_STRT,END to factory default also fail with the same output: "Expected value for Option Byte [...], found [...]"
Overall the option bytes seem pretty out of order - is there a certain order I have to follow to change them back from my current configuration (first message) to a configuration where e.g. BOOT_UBE can be changed?
Thank you very much for your help!
Best regards
2025-08-01 7:47 AM
Update: @Jocelyn RICARD
I compared the option bytes of a brand-new Nucleo-H563ZI with thos of the "broken" board. Aside from BOOT_UBE and PRODUCT_STATE, every other field is identical. I am using STM32CubeProgrammer V2.20.0
Factory new Nucleo-H563ZI:
{
"deviceId" : 1156,
"bitNameToValue" : {
"PRODUCT_STATE" : 237,
"BOR_LEV" : 0,
"BORH_EN" : 0,
"IO_VDD_HSLV" : 0,
"IO_VDDIO2_HSLV" : 0,
"IWDG_STOP" : 1,
"IWDG_STDBY" : 1,
"BOOT_UBE" : 180,
"SWAP_BANK" : 0,
"IWDG_SW" : 1,
"NRST_STOP" : 1,
"NRST_STDBY" : 1,
"TZEN" : 195,
"USBPD_DIS" : 1,
"SRAM2_ECC" : 1,
"SRAM3_ECC" : 1,
"BKPRAM_ECC" : 1,
"SRAM2_RST" : 1,
"SRAM1_3_RST" : 1,
"NSBOOTADD" : 524288,
"NSBOOT_LOCK" : 195,
"SECBOOT_LOCK" : 0,
"SECBOOTADD" : 0,
"SECWM1_STRT" : 0,
"SECWM1_END" : 127,
"WRPSGn1" : 4294967295,
"SECWM2_STRT" : 0,
"SECWM2_END" : 127,
"WRPSGn2" : 4294967295,
"LOCKBL" : 0,
"EDATA1_EN" : 0,
"EDATA1_STRT" : 0,
"EDATA2_EN" : 0,
"EDATA2_STRT" : 0,
"HDP1_STRT" : 1,
"HDP1_END" : 0,
"HDP2_STRT" : 1,
"HDP2_END" : 0
}
}"Broken" Nucleo-H563ZI:
{
"deviceId" : 1156,
"bitNameToValue" : {
"PRODUCT_STATE" : 23,
"BOR_LEV" : 0,
"BORH_EN" : 0,
"IO_VDD_HSLV" : 0,
"IO_VDDIO2_HSLV" : 0,
"IWDG_STOP" : 1,
"IWDG_STDBY" : 1,
"BOOT_UBE" : 195,
"SWAP_BANK" : 0,
"IWDG_SW" : 1,
"NRST_STOP" : 1,
"NRST_STDBY" : 1,
"TZEN" : 195,
"USBPD_DIS" : 1,
"SRAM2_ECC" : 1,
"SRAM3_ECC" : 1,
"BKPRAM_ECC" : 1,
"SRAM2_RST" : 1,
"SRAM1_3_RST" : 1,
"NSBOOTADD" : 524288,
"NSBOOT_LOCK" : 195,
"SECBOOT_LOCK" : 0,
"SECBOOTADD" : 0,
"SECWM1_STRT" : 0,
"SECWM1_END" : 127,
"WRPSGn1" : 4294967295,
"SECWM2_STRT" : 0,
"SECWM2_END" : 127,
"WRPSGn2" : 4294967295,
"LOCKBL" : 0,
"EDATA1_EN" : 0,
"EDATA1_STRT" : 0,
"EDATA2_EN" : 0,
"EDATA2_STRT" : 0,
"HDP1_STRT" : 1,
"HDP1_END" : 0,
"HDP2_STRT" : 1,
"HDP2_END" : 0
}
}
2025-08-01 8:59 AM
Hi @jho ,
you should first re-enable the TrustZone before changing security related option bytes.
Best regards
Jocelyn
2025-08-03 11:46 AM
Hi @Jocelyn RICARD ,
re-enabling TrustZone and then changing BOOT_UBE also did not succeed:
20:34:16 : OPTION BYTE PROGRAMMING VERIFICATION:
20:34:16 : Error: Expected value for Option Byte "BOOT_UBE": 0xB4, found: 0xC3
20:34:16 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCHNote: I am connected via Hot Plug on Access Port 1 - is this fine?
The following log shows the Secure Firmware Install process. Is there any indication why the regression is now failing, and why the expected firmware in the SFI image did not flash correctly?
15:23:27 : SFI header information :
15:23:27 : SFI protocol version : 2
15:23:27 : SFI total number of areas : 4
15:23:27 : SFI image version : 0
15:23:27 : SFI Areas information :
15:23:27 : Parsing Area 1/4 :
15:23:27 : Area type : H
15:23:27 : Area size : 16
15:23:27 : Area destination address : 0x0
15:23:27 : Parsing Area 2/4 :
15:23:27 : Area type : O
15:23:27 : Area size : 112
15:23:27 : Area destination address : 0xFFD0100
15:23:27 : Parsing Area 3/4 :
15:23:27 : Area type : F
15:23:27 : Area size : 24416
15:23:27 : Area destination address : 0x8000000
15:23:27 : Parsing Area 4/4 :
15:23:27 : Area type : C
15:23:27 : Area size : 36
15:23:27 : Area destination address : 0x0
15:23:27 : Parsed File SUCCESS
15:23:31 : UPLOADING ...
15:23:31 : Size : 4 Bytes
15:23:31 : Address : 0xBF960CC
15:23:31 : Read progress:
15:23:31 : Data read successfully
15:23:31 : Time elapsed during the read operation is: 00:00:00.013
15:23:31 : Requesting Chip Certificate from device ...
15:23:31 : Reading chip Certificate finished
15:23:31 : Get Certificate done successfully
15:23:31 : requesting license for the current STM32 device
15:23:31 : Init Communication ...
15:23:31 : P11 lib initialization Success!
15:23:31 : Opening session with slot ID 1...
15:23:31 : Succeed to Open session with reader slot ID 1
15:23:32 : Succeed to generate license for the current STM32 device
15:23:32 : Closing session with reader slot ID 1...
15:23:32 : Session closed with reader slot ID 1
15:23:32 : Closing communication with HSM...
15:23:32 : Communication closed with HSM
15:23:32 : Succeed to get License for Firmware from HSM slot ID 1
15:23:32 : Starting Firmware Install operation...
15:23:32 : Warning: Option Byte: BOOT_UBE, value: 0xB4, was not modified.
15:23:32 : Warning: Option Bytes are unchanged, Data won't be downloaded
15:23:32 : Time elapsed during option Bytes configuration: 00:00:00.014
15:23:32 : Reconnecting...
15:23:34 : Reconnected !
15:23:34 : Reconnecting...
15:23:35 : Reconnected !
15:23:35 : Time elapsed during option Bytes configuration: 00:00:02.542
15:23:36 : ST-LINK SN : 56FF6D065182525038591787
15:23:36 : ST-LINK FW : V2J45S7
15:23:36 : Board : --
15:23:36 : Voltage : 3.24V
15:23:36 : SWD freq : 4000 KHz
15:23:36 : Connect mode: Normal
15:23:36 : Reset mode : Hardware reset
15:23:36 : Device ID : 0x484
15:23:36 : Revision ID : Rev X
15:23:36 : Reconnecting...
15:23:37 : Reconnected !
15:23:37 : Time elapsed during option Bytes configuration: 00:00:01.284
15:23:37 : Warning: Option Byte: SECBOOT_LOCK, value: 0xC3, was not modified.
15:23:37 : Warning: Option Bytes are unchanged, Data won't be downloaded
15:23:37 : Time elapsed during option Bytes configuration: 00:00:00.014
15:23:37 : Warning: Option Byte: SECBOOTADD, value: 0xC0000, was not modified.
15:23:37 : Warning: Option Byte: SECWM1_END, value: 0x7F, was not modified.
15:23:37 : Warning: Option Byte: SECWM1_STRT, value: 0x0, was not modified.
15:23:37 : Warning: Option Byte: SECWM2_END, value: 0x7F, was not modified.
15:23:37 : Warning: Option Byte: SECWM2_STRT, value: 0x0, was not modified.
15:23:37 : Warning: Option Byte: SRAM1_3_RST, value: 0x1, was not modified.
15:23:37 : Reconnecting...
15:23:39 : Reconnected !
15:23:39 : Time elapsed during option Bytes configuration: 00:00:01.290
15:23:40 : ST-LINK SN : 56FF6D065182525038591787
15:23:40 : ST-LINK FW : V2J45S7
15:23:40 : Board : --
15:23:40 : Voltage : 3.24V
15:23:40 : SWD freq : 4000 KHz
15:23:40 : Connect mode: Normal
15:23:40 : Reset mode : Hardware reset
15:23:40 : Device ID : 0x484
15:23:40 : Revision ID : Rev X
15:23:40 : ST-LINK SN : 56FF6D065182525038591787
15:23:40 : ST-LINK FW : V2J45S7
15:23:40 : Board : --
15:23:40 : Voltage : 3.24V
15:23:40 : Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
15:23:40 : Reconnecting...
15:23:41 : Reconnected !
15:23:42 : Reconnecting...
15:23:43 : Reconnected !
15:23:43 : Time elapsed during option Bytes configuration: 00:00:03.293
15:23:44 : ST-LINK SN : 56FF6D065182525038591787
15:23:44 : ST-LINK FW : V2J45S7
15:23:44 : Board : --
15:23:44 : Voltage : 3.23V
15:23:44 : SWD freq : 4000 KHz
15:23:44 : Connect mode: Hot Plug
15:23:44 : Reset mode : Hardware reset
15:23:44 : Device ID : 0x484
15:23:44 : Revision ID : Rev X
15:23:44 : Installing RSSe
15:23:44 : Opening and parsing file: RSSe_SFI_H56x_H573_v3.1.0.bin
15:23:44 : Memory Programming ...
15:23:44 : File : RSSe_SFI_H56x_H573_v3.1.0.bin
15:23:45 : Size : 55.56 KB
15:23:45 : Address : 0x2007CCDF
15:23:45 : File segment @0x2007CCDF is not 16-bytes aligned. It will be aligned to @0x2007CCD0
15:23:45 : Erasing memory corresponding to sector 0:
15:23:45 : Download in Progress:
15:23:45 : File download complete
15:23:45 : Time elapsed during download operation: 00:00:00.384
15:23:45 : MCU Reset
15:23:46 : ST-LINK SN : 56FF6D065182525038591787
15:23:46 : ST-LINK FW : V2J45S7
15:23:46 : Board : --
15:23:46 : Voltage : 3.23V
15:23:46 : SWD freq : 4000 KHz
15:23:46 : Connect mode: Hot Plug
15:23:46 : Reset mode : Hardware reset
15:23:46 : Device ID : 0x484
15:23:46 : Revision ID : Rev X
15:23:46 : Get RSSe status...
15:23:47 : RSS version = 2.2.0
15:23:47 : RSSe version = 3.1.0
15:23:47 : Starting SFI
15:23:47 : Processing license...
15:23:47 : Get RSSe status...
15:23:47 : Processing Image Header
15:23:47 : Get RSSe status...
15:23:47 : Processing Area 1...
15:23:50 : Get RSSe status...
15:23:50 : Area Address = 0x0
15:23:50 : Area Type = H
15:23:50 : Processing Area 2...
15:23:51 : Get RSSe status...
15:23:51 : Area Address = 0xFFD0100
15:23:51 : Area Type = O
15:23:51 : Processing Area 3...
15:23:52 : Get RSSe status...
15:23:52 : Area Address = 0x8000000
15:23:52 : Area Type = F
15:23:52 : Processing Area 4...
15:23:52 : ---- Is Last SFI Area !! ----
15:23:52 : Can not verify last area
15:23:52 : Area Address = 0x0
15:23:52 : Area Type = C
15:23:52 : SFI Process Finished!
15:23:52 : SFI file Install Operation Success
15:25:18 : Disconnected from device.Best regards
2025-08-05 6:16 AM
Hello @jho ,
It looks like something happened during your SFI testing that led to this device state.
I would guess that, at some point, the SFI was interrupted at the wrong time.
Another possibility is the sfi image you have built that show a possible issue: the size of Area 4 of type C 36 is not normal. This area contains the option bytes to write at the end of the SFI process. This may have generated this issue.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.