2024-09-06 4:04 AM - last edited on 2024-09-09 12:38 AM by mƎALLEm
Hello,
I'm working on STM32H7B3I-EVAL with STM32CubeIDE. I would like to write in the OSPI, so I made the following code:
void OSPI_Write(uint32_t address, uint8_t *data, uint32_t size) {
OSPI_RegularCmdTypeDef sCommand;
// Désactivation du mode mappé
HAL_OSPI_Abort(&hospi1);
// Configuration de la commande pour l'écriture en mode indirect
sCommand.OperationType = HAL_OSPI_OPTYPE_WRITE_CFG;
sCommand.FlashId = HAL_OSPI_FLASH_ID_1;
sCommand.Instruction = MX25LM51245G_OCTA_WRITE_ENABLE_CMD;
sCommand.InstructionMode = HAL_OSPI_INSTRUCTION_8_LINES;
sCommand.Address = address;
sCommand.AddressMode = HAL_OSPI_ADDRESS_8_LINES;
sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
sCommand.NbData = size;
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_OSPI_DQS_DISABLE;
// Envoye de la commande d'écriture
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) { //5s
Error_Handler();
}
// Écrire les données dans la mémoire
if (HAL_OSPI_Transmit(&hospi1, data, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) {
Error_Handler();
}
// Attendre que l'opération soit terminée
OSPI_AutoPollingMemReady(&hospi1);
}
void OSPI_AutoPollingMemReady(OSPI_HandleTypeDef *hospi) {
OSPI_AutoPollingTypeDef sConfig;
// Configuration pour la lecture du statut de la mémoire pour vérifier si elle est prête
sConfig.Match = 0x00;
sConfig.Mask = 0x01;
sConfig.MatchMode = HAL_OSPI_MATCH_MODE_AND;
sConfig.Interval = 0x10;
sConfig.AutomaticStop = HAL_OSPI_AUTOMATIC_STOP_ENABLE;
OSPI_RegularCmdTypeDef sCommand;
sCommand.Instruction = 0x05;
sCommand.InstructionMode= HAL_OSPI_INSTRUCTION_8_LINES;
sCommand.AddressMode = HAL_OSPI_ADDRESS_NONE;
sCommand.DataMode = HAL_OSPI_DATA_8_LINES;
sCommand.NbData = 1;
HAL_OSPI_Command(hospi, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
HAL_OSPI_AutoPolling(hospi, &sConfig, HAL_OSPI_TIMEOUT_DEFAULT_VALUE);
}
Sorry the comments are in french.
The problem is that it can't write to the OSPI, on the first if it does Error_Handler.
Could you please help me to understand where the error comes from?
Solved! Go to Solution.
2024-09-06 9:11 AM
>>I still get the same thing
That's not helpful. Which part is failing, what line, what error? Make sure the setting passed are consistent with the mode the memory is in. You can't randomly mix-n-match. If you're going to cut-n-paste code you're going to have to pay attention to ALL the details for it to have some chance of working.
The Write Enable has no address or data component
2024-09-06 5:11 AM
Where does Error_Handler get called? Look at the call stack and go back to see where/why it's called and correct. Step through the functions to see where it bails out.
2024-09-06 5:22 AM
Thank you for your reply
it is called here ”
if (HAL_OSPI_Command(&hospi1, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) { Error_Handler();
}"
Except that normally, if it's written properly, it's not supposed to call Error_Handler.
I don't understand why it can't write.
2024-09-06 5:57 AM
Step into that function and step line by line and see where it exits. Don't treat it as a black box. Probably something in the sCommand structure is invalid or hospi1 state is not as expected.
2024-09-06 6:31 AM - edited 2024-09-06 6:32 AM
nous entrons dans la fonction et elle reste bloquée dans la boucle while(1) :
Savez-vous comment je peux savoir d’où vient l’erreur ?
I'm sorry, I'm just starting out and I don't speak English very well.
2024-09-06 6:40 AM
OSPI_RegularCmdTypeDef sCommand = {0}; // Clear the auto variables for consistency of usage
Step 1 : Write Enable, just the Command
Step 2 :Page Program, with the Address / Data
2024-09-06 6:58 AM
Thanks for your help.
I modified my code like this :
I still get the same thing.
2024-09-06 9:11 AM
>>I still get the same thing
That's not helpful. Which part is failing, what line, what error? Make sure the setting passed are consistent with the mode the memory is in. You can't randomly mix-n-match. If you're going to cut-n-paste code you're going to have to pay attention to ALL the details for it to have some chance of working.
The Write Enable has no address or data component