2019-03-31 2:48 PM
STM32F413, CubeMx 5.1.0 plugin to SW4STM32, with Library STMR32Cube_FW_F4_V1.24.0.
In previous versions we were able to set the transfer direction for I2S4,I2S5 half duplex channels. In the above version only transmit can be selected and the ability to select receive mode has been incorrectly removed. This is a regression test failure.
2019-04-02 7:07 AM
Hello @Kent Swan ,
After check using same versions of CubeMx and CubeF4, we have the ability to select transmit and receive mode.
Can you please share your ioc file to check more this behavior?
Regards,
Imen
2019-04-02 7:53 AM