cancel
Showing results for 
Search instead for 
Did you mean: 

why is there such a bad attitude to writing documentation ? check the attach

why is there such a bad attitude to writing documentation ?

English is not the main language for me, but even I see a lot of spelling errors in the documentation, are you forbidden to check ?

7 REPLIES 7

Because it is a chore, and the people writing it are probably not the people building/designing it.

Logical thing here is a flop-flop to synchronize the secondary signal with the carrier so the AND gate doesn't get artifacts and beat/modulation related to disparities in the frequencies being mixed.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

In general, because whoever is doing the document is probably rewarded for getting the document done, but not so much for making it perfect. And it is a 150 page document, there are going to be issues. Might also be the figure didn't translate to PDF properly. Anyone who has converted things to PDF runs into issues. I have 3 ways to create a PDF from a document on my computer and all 3 ways produce slightly different PDFs. Doesn't make sense, but that's how it is.

If you're really interested in the infrared transmitter, this explains it better:

https://www.st.com/resource/en/application_note/dm00271524-implementation-of-transmitters-and-receivers-for-infrared-remote-control-protocols-with-stm32cube-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".
I can understand everything, but the authority and face of the company suffers when users see incomplete documents. After the PDF is created, it is normal practice to give it to different people for careful reading. The ST company is not small enough to have problems with finances and pay people for a detailed review of documentation. чт, 12 но�?б. 2020 г. в 07:12, ST Community :

Judging from the majority of questions here, I bet ST is financially rewarded a lot more for adding new features into CubeMX than doing a detailed review of documentation. It's never a question of do X or not do X, it's a question of where to put resources. Want more documentation reviews? Something else suffers. Always a choice.

If you feel a post has answered your question, please click "Accept as Solution".
kent-dorfman
Associate II

I too am less than impressed with STM documentation and tools.  I've been doing close-to-hardware programming since around 1990 and the tools and support docs come across as amateurish.

The guy who went postal with his "don't make us log in to use the tools" rant said everything I wanted to say, and then some.

I own one U585-IOT2a board that I use to create "tickle the hardware" apps for my test harnesses and I have spent way too much wasted time due to poorly thought out and overly convoluted support code layering, and documentation that is way too often, just plain wrong.

I'm about convinced myself to create a hardware tickler on my Xilinx Zynq board and throw the STM32 out the nearest air-lock.

 

JPeac.1
Senior

I often complained about documentation...until I had to write the technical manual.  I discovered it isn't nearly as easy as it seems.  Writing a manual after the fact means you have to recall all the design criteria that was never written down and lay it out in a manner that's hopefully easy to comprehend.  And when you finish, there's no one to edit it, because you're the only expert.

Grammar and spelling checks help, but they do miss glaring errors.  So you proofread, except you miss the errors because you've seen the text so many times the words blur together.  Your mind skips past those spelling errors.

On the whole I've found ST reference manuals to be very helpful, other than a few cases like their arcane USB.  The Cube tools are a nightmare, so much that I never used them.  Doxygen used on the old ST Peripheral Library was great for some internal code documentation but worthless to anyone but the programmers who wrote it in the first place. 

I've used ST controllers since the ARM7TDMI, before the Cortex series.  The old SPL Library concept worked well until ST decided to be clever and package a "one size fits all" code generation package that does little more than encourage migration to Linux and A series.  I'm sure this made economic sense so I can't criticize ST for business decisions.  It does impose a technical debt in that the firmware embedded in a project is no longer maintainable solely by developers.  I'm not willing to pay that price, since I staked my expertise and reputation on the product I delivered to my employer (not to mention the massive headaches it causes in regulated industries).

As for the bad attitude in general, I had one of those "AH HA" moments when a Windows app programmer told me I was wrong to comment code because the functionality should be self-evident based on how the variables were named.  He was taught to do this at university.  Writing is drudgery, coding is exciting.  Until, of course, your manager hands you that brilliant code with the assignment to maintain it, since Cowboy Coder has left for some flavor of the day website.

To answer your question, have patience and be grateful for whatever you get for documentation.  The days of the ten foot high stacks of OS/360 or the "gray wall" of DEC VMS documentation died forty years ago.  If you're lucky the worst you will encounter are spelling errors.  Does anyone remember when ST changed one of the STM32F4 pins from Vcc to GND between versions of the datasheet?  Those kinds of documentation "features" are the ones that should keep you awake at night.

  Jack Peacock

  It does impose a technical debt in that the firmware embedded in a project is no longer maintainable solely by developers. 

How come? How this is different from (say) Linux & yocto?  Even if the "cube" libraries are not quite production quality (even not speaking about the generated code) - developers get the complete source and can maintain it.