2024-11-07 12:59 AM - last edited on 2024-11-07 4:58 AM by Andrew Neil
Hi, I am using STM32H563 Nucleo board, and found the PLL1VCOSEL bit of RCC PLL clock source selection register.
There are duplicates in the settings.
Does anyone know why is the settings duplicates?
I would like to know why and use case.
2024-11-07 4:51 AM - edited 2024-11-08 2:44 AM
There is no duplication in the settings. The PLL proposes 2 VCO settings:
I hope I have answered your question.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 4:52 AM
I do not see a duplicate setting.
The medium VCO range setting needs less current. See datasheet 5.3.10