2020-10-28 06:48 AM
#define STARTUP_MSG "Test Rx-interrupt\n"
#include <stdio.h>
#include "stm32f4xx_hal.h"
#define get_RTC HAL_GetTick
#define LED_inv HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5)
#define LED_on HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_SET)
#define LED_off HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET)
void waitXms( uint32_t );
void USART1_IRQHandler( void );
void USART3_IRQHandler( void );
void UART4_IRQHandler( void );
void uart1_init( void );
void uart2_init( void );
void uart3_init( void );
void uart4_init( void );
UART_HandleTypeDef hU1, hU2, hU3, hU4;
/*---------------------------------------------------------------------------*/
/* UART1 Interrupt Service Routine */
void USART1_IRQHandler( void ) {
uint8_t uc;
uc = (&hU1)->Instance->DR; // Read data and clear flag
putchar( uc ); // Echo to debug-uart
LED_inv; // Toggle LED to check if program comes here
}
void uart1_init( void ) {
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_9 | GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // PA9 = TxD1, PA10 = RxD1 Alternate Function 8
__USART1_CLK_ENABLE();
hU1.Instance = USART1;
hU1.Init.BaudRate = 38400;
hU1.Init.WordLength = UART_WORDLENGTH_8B;
hU1.Init.StopBits = UART_STOPBITS_1;
hU1.Init.Parity = UART_PARITY_NONE;
hU1.Init.Mode = UART_MODE_TX_RX;
hU1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hU1.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&hU1);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(USART1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART1_IRQn);
__HAL_USART_ENABLE_IT(&hU1, UART_IT_RXNE);
}
/*---------------------------------------------------------------------------*/
void uart2_init( void ) {
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);// PA2 = TxD2 Alternate Function 8
// PA3 = RxD2 Alternate Function 8
__USART2_CLK_ENABLE();
hU2.Instance = USART2;
hU2.Init.BaudRate = 38400;
hU2.Init.WordLength = UART_WORDLENGTH_8B;
hU2.Init.StopBits = UART_STOPBITS_1;
hU2.Init.Parity = UART_PARITY_NONE;
hU2.Init.Mode = UART_MODE_TX_RX;
hU2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hU2.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&hU2);
// No interrupt for debug-USART
}
/*---------------------------------------------------------------------------*/
/* UART3 Interrupt Service Routine */
void USART3_IRQHandler( void ) {
uint8_t uc;
uc = (&hU3)->Instance->DR; // Read data and clear flag
putchar( uc ); // Echo to debug-uart
LED_inv; // Toggle LED to check if program comes here
}
void uart3_init( void ) {
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOC_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); // PC5 = RxD3 Alternate Function 7
__USART3_CLK_ENABLE();
hU3.Instance = USART3;
hU3.Init.BaudRate = 38400;
hU3.Init.WordLength = UART_WORDLENGTH_8B;
hU3.Init.StopBits = UART_STOPBITS_1;
hU3.Init.Parity = UART_PARITY_NONE;
hU3.Init.Mode = UART_MODE_RX; // Only receiver
hU3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hU3.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&hU3);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART3_IRQn);
__HAL_USART_ENABLE_IT(&hU3, UART_IT_RXNE);
}
/*---------------------------------------------------------------------------*/
/* UART4 Interrupt Service Routine */
void UART4_IRQHandler( void ) {
uint8_t uc;
uc = (&hU4)->Instance->DR; // Read data and clear flag
putchar( uc ); // Echo to debug-uart
LED_inv; // Toggle LED to check if program comes here
}
void uart4_init( void ) {
GPIO_InitTypeDef GPIO_InitStruct;
__GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_0;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // PA0 = TxD4 Alternate Function 8
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // PA1 = RxD4 Alternate Function 8
__UART4_CLK_ENABLE();
hU4.Instance = UART4;
hU4.Init.BaudRate = 38400;
hU4.Init.WordLength = UART_WORDLENGTH_8B;
hU4.Init.StopBits = UART_STOPBITS_1;
hU4.Init.Parity = UART_PARITY_NONE;
hU4.Init.Mode = UART_MODE_TX_RX;
hU4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hU4.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&hU4);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(UART4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(UART4_IRQn);
__HAL_USART_ENABLE_IT(&hU4, UART_IT_RXNE);
}
/*---------------------------------------------------------------------------*/
int main( void ) {
GPIO_InitTypeDef GPIO_InitStruct;
// Reset of all peripherals, Initializes the Flash interface and the Systick.
HAL_Init();
__HAL_RCC_GPIOA_CLK_ENABLE();
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);// PA5 == LED
uart2_init(); // Debug-UART (putchar)
printf( STARTUP_MSG );
//uart1_init(); // OK
//uart3_init(); // OK
uart4_init(); // NOT WORKING
while(1) {
//LED_inv;
waitXms( 500 );
}
}
/* ------------------------------------------------------------------------- */
// Debug goes to Nucleo-standard UART2/TxD2/PA2
int putchar( int val ) {
if( 10 == val ) putchar( 13 );
while( __HAL_UART_GET_FLAG( &hU2, UART_FLAG_TC) != SET); // Wait for empty register
(&hU2)->Instance->DR = val; // Direct write to register
return val;
}
/* ------------------------------------------------------------------------ */
void waitXms( uint32_t loop ) {
uint32_t ul;
while( loop ) {
for( ul=0; ul < 10000U; ul++ ) asm(" nop");
loop--;
}
}
/*----------------------------------------------------------------------------*/
Solved! Go to Solution.
2020-10-28 01:53 PM
F446RE not an F1 series
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; // USE GPIO_MODE_AF_PP
2020-10-28 11:40 AM
Include your chip number.
What does "not working" mean in particular? How do you know it's not working?
2020-10-28 01:53 PM
F446RE not an F1 series
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; // USE GPIO_MODE_AF_PP
2020-10-29 05:13 AM
Thanks clive1,
now we got it to work! :-)