2019-08-28 07:46 AM
Hello,
according to the product selector on the ST website, the only MCU from L412 series that has SMPS and is in production is STM32L412RB with 64 pins in LQFP and UFBGA package.
In the product specification v6, on p57 at the PIN definitions table, I can find only WLCSP36 SMPS and LQFP64 SMPS. in some supplies there are UFBGA, LQFP and QFN.
thank you.
Solved! Go to Solution.
2019-08-29 01:45 AM
Please check CubeMX tool, select your MCU, and open new project, you will find see expected pinout for LQFP48 SMPS.
In this tool, you can see marketing status as well. And so far, LQFP48 SMPS (STM32L412CBTx-P) is not flagged as active.
Anyways, officially, if it is not listed on ST website, then it is not available.
You should contact your local ST office to have more information about (future) availability.
2019-08-28 09:01 AM
2019-08-28 10:56 PM
thank you, but this is the same document I was referring to. On p.56/57 there are only only WLCSP36 SMPS and LQFP64 SMPS described. Any other idea? I would need for 48 pin LQFP and it is missing from this specification file.
2019-08-29 01:45 AM
Please check CubeMX tool, select your MCU, and open new project, you will find see expected pinout for LQFP48 SMPS.
In this tool, you can see marketing status as well. And so far, LQFP48 SMPS (STM32L412CBTx-P) is not flagged as active.
Anyways, officially, if it is not listed on ST website, then it is not available.
You should contact your local ST office to have more information about (future) availability.
2019-08-29 03:32 AM
thank you, it is clear now
2020-10-26 12:26 AM
Where can I find a pinout for STM32L412CBU6P part (LQFP48 with ext. SMPS)?
This part is available in product selector on the ST site, Device Configuration Tool in STM32CubeIDE, but not in the DS (https://www.st.com/resource/en/datasheet/stm32l412cb.pdf).
2021-03-12 02:27 AM
Hello,
Same questions, will you update the DS please ?
2021-03-31 07:02 AM
Hi @OGUIL.1 , @APros.1 ,
A new datasheet will be published soon on the ST website containing this update =).
Imen
2021-03-31 08:03 AM
Thanks, Imen.
JW
2022-04-23 12:52 AM
Hi Imen,
It's been more than a year, and there's still no new datasheet containing the 48-pin version with SMPS.The currently publishe one is Rev 8, of 03-Nov-2020.
Can you please push this a little bit further?
Thanks,
Jan
@Imen DAHMEN