2023-04-03 01:19 AM
Good afternoon!
Our university bought approximatively 9 or 10 B-L4S5I-IOT01A Discovery kits for lab/projects at Embedded Systems course. I found that for this board I have no examples. I installed 30 GB of software/support package on my laptop.
On STM32 board site is written:
Comprehensive free software libraries and examples available with the STM32Cube MCU Package
Why I cannot find examples when I create a project with STM32Cube IDE?
I want to develop some labs using FreeRTOS and wireless connection protocols without FreeRTOS , but the examples are missing.
To view the temperature from sensor mounted on the board I created an example using libraries from STM32Cube_FW_L4_V1.17.2 package
How can I add Comprehensive examples to STM32Cube IDE.?
I am not happy with situation which create difficulties for developing labs for students.
Solved! Go to Solution.
2023-04-03 01:52 AM
Hello @Community member and welcome to the Community :)
I recommend you review the WiFi demo app showing the temperature sensor on a web page:
STM32CubeL4/Projects/B-L4S5I-IOT01A/Applications/WiFi/WiFi_HTTP_Server at master ·
You will find BSP drivers (easy-to-use) available for various sensors: STM32CubeL4/Drivers/BSP/B-L4S5I-IOT01 at master - GitHub.
You can also get inspired from available applications here: STM32CubeL4/Projects/B-L475E-IOT01A at master · GitHub
Imen
2023-04-03 01:52 AM
Hello @Community member and welcome to the Community :)
I recommend you review the WiFi demo app showing the temperature sensor on a web page:
STM32CubeL4/Projects/B-L4S5I-IOT01A/Applications/WiFi/WiFi_HTTP_Server at master ·
You will find BSP drivers (easy-to-use) available for various sensors: STM32CubeL4/Drivers/BSP/B-L4S5I-IOT01 at master - GitHub.
You can also get inspired from available applications here: STM32CubeL4/Projects/B-L475E-IOT01A at master · GitHub
Imen
2024-01-14 02:37 AM
Hi
If you are still looking for lab sheets on this "B-L4S5I-IOT01A Discovery kit", I can share the material.
I have developed a lab manual for an "embedded system" course using the kit in question.
The material is mainly for the educational needs of the BS level students
2024-01-14 08:06 PM
Contents of the training manual on the "B-L4S5I-IOT01A Discovery" kit.
2024-02-08 03:12 PM
Wow!
I'm also trying to master the STM32 platform with the help of this particular board.
Where I could find these labs to try on?
2024-05-15 09:31 PM
I'd greatly appreciate it if you could share the lab manual for the 'B-L4S5I-IOT01A Discovery kit.' It sounds like it would be incredibly helpful. Thank you so much in advance
2024-05-16 10:21 AM
2024-05-16 10:35 AM
Try the below-listed link to access the material,
https://drive.google.com/drive/u/2/folders/19yKII2xydTZjS4XE1g5-YpHA2sRcXnTD
2024-05-16 10:36 AM
Try the below listed link to access the material
https://drive.google.com/drive/u/2/folders/19yKII2xydTZjS4XE1g5-YpHA2sRcXnTD
2024-05-16 09:40 PM
I can't find all the topic you have mentioned above in the provided google drive