cancel
Showing results for 
Search instead for 
Did you mean: 

Where are the .ioc files for STSW-STLKT01 sample programs?

HCohe.1
Associate III

According to the data brief STSW-STLKT01 Embedded software samples for SensorTile (DB2962) the sample projects are "Built on STM32Cube software technology, it includes all the low level drivers to manage the on-board devices and system-level interfaces.", however, I do not see any of the .ioc files present. Please provide them so I can migrate existing applications to the SensorTile platform.

1 REPLY 1
HCohe.1
Associate III

If the .ioc files are not available, can you provide instructions for using CubeMX to generate a skeleton app for the STM32L4 MCU and BlueNRG controller that runs on the STEVAL-STLKT01V1?