2022-04-06 07:54 AM
According to the data brief STSW-STLKT01 Embedded software samples for SensorTile (DB2962) the sample projects are "Built on STM32Cube software technology, it includes all the low level drivers to manage the on-board devices and system-level interfaces.", however, I do not see any of the .ioc files present. Please provide them so I can migrate existing applications to the SensorTile platform.
2022-04-06 08:06 AM
If the .ioc files are not available, can you provide instructions for using CubeMX to generate a skeleton app for the STM32L4 MCU and BlueNRG controller that runs on the STEVAL-STLKT01V1?