2020-04-01 6:25 AM
Hi Folks,
i'm working with the STM32H750 controller. At the moment i'm trying to get the ADC working with the DMA in a Peripheral to Memory Mode.
Since i've no idea how to do this, i've started to checking the HAL functions and found the HAL_DMA_Start() function which leads to the DMA_SetConfig() function.
Here's the code from that:
/**
* @brief Sets the DMA Transfer parameter.
* @param hdma: pointer to a DMA_HandleTypeDef structure that contains
* the configuration information for the specified DMA Stream.
* @param SrcAddress: The source memory Buffer address
* @param DstAddress: The destination memory Buffer address
* @param DataLength: The length of data to be transferred from source to destination
* @retval None
*/
static void DMA_SetConfig(DMA_HandleTypeDef *hdma, uint32_t SrcAddress, uint32_t DstAddress, uint32_t DataLength)
{
/* calculate DMA base and stream number */
DMA_Base_Registers *regs_dma = (DMA_Base_Registers *)hdma->StreamBaseAddress;
BDMA_Base_Registers *regs_bdma = (BDMA_Base_Registers *)hdma->StreamBaseAddress;
if(IS_DMA_DMAMUX_ALL_INSTANCE(hdma->Instance) != 0U) /* No DMAMUX available for BDMA1 */
{
/* Clear the DMAMUX synchro overrun flag */
hdma->DMAmuxChannelStatus->CFR = hdma->DMAmuxChannelStatusMask;
if(hdma->DMAmuxRequestGen != 0U)
{
/* Clear the DMAMUX request generator overrun flag */
hdma->DMAmuxRequestGenStatus->RGCFR = hdma->DMAmuxRequestGenStatusMask;
}
}
if(IS_DMA_STREAM_INSTANCE(hdma->Instance) != 0U) /* DMA1 or DMA2 instance */
{
/* Clear all interrupt flags at correct offset within the register */
regs_dma->IFCR = 0x3FUL << (hdma->StreamIndex & 0x1FU);
/* Clear DBM bit */
((DMA_Stream_TypeDef *)hdma->Instance)->CR &= (uint32_t)(~DMA_SxCR_DBM);
/* Configure DMA Stream data length */
((DMA_Stream_TypeDef *)hdma->Instance)->NDTR = DataLength;
/* Peripheral to Memory */
if((hdma->Init.Direction) == DMA_MEMORY_TO_PERIPH)
{
/* Configure DMA Stream destination address */
((DMA_Stream_TypeDef *)hdma->Instance)->PAR = DstAddress;
/* Configure DMA Stream source address */
((DMA_Stream_TypeDef *)hdma->Instance)->M0AR = SrcAddress;
}
/* Memory to Peripheral */
else
{
/* Configure DMA Stream source address */
((DMA_Stream_TypeDef *)hdma->Instance)->PAR = SrcAddress;
/* Configure DMA Stream destination address */
((DMA_Stream_TypeDef *)hdma->Instance)->M0AR = DstAddress;
}
}
else if(IS_BDMA_CHANNEL_INSTANCE(hdma->Instance) != 0U) /* BDMA instance(s) */
{
/* Clear all flags */
regs_bdma->IFCR = (BDMA_ISR_GIF0) << (hdma->StreamIndex & 0x1FU);
/* Configure DMA Channel data length */
((BDMA_Channel_TypeDef *)hdma->Instance)->CNDTR = DataLength;
/* Peripheral to Memory */
if((hdma->Init.Direction) == DMA_MEMORY_TO_PERIPH)
{
/* Configure DMA Channel destination address */
((BDMA_Channel_TypeDef *)hdma->Instance)->CPAR = DstAddress;
/* Configure DMA Channel source address */
((BDMA_Channel_TypeDef *)hdma->Instance)->CM0AR = SrcAddress;
}
/* Memory to Peripheral */
else
{
/* Configure DMA Channel source address */
((BDMA_Channel_TypeDef *)hdma->Instance)->CPAR = SrcAddress;
/* Configure DMA Channel destination address */
((BDMA_Channel_TypeDef *)hdma->Instance)->CM0AR = DstAddress;
}
}
else
{
/* Nothing To Do */
}
}
First of all, the commentary is faulty. When it says /* Peripheral to Memory */ it is checking for "== MEMORY_TO_PERIPH" so that is wrong right away. But that's not the problem here: I don't quiet now, what address should be entered for the source of the DMA transfer. In my case a want to get a specific number of samples from ADC1_CH0 to a given memspace (initiatet with a variable and referenced by a pointer of course).
Can you maybee give me some input to get this done? =)
Thanks in advance,
kind regards
Tony
2020-04-01 7:36 AM