2019-10-09 5:07 AM
I use stm32l496. before entering the low power run mode I set the output but when micro enter lprun the output is reset.
I want to know what the status of the outputs is at low power mode?
and
can the outputs be changed or read?
thank's.
2019-10-09 10:08 PM
From the manual:
In Low-power run mode, all I/O pins keep the same state as in Run mode.
I see no reason why they could not be changed or read in LP run mode.
2019-10-09 10:50 PM
I pasted my code.
Is my code wrong?
thanks.
HAL_GPIO_WritePin(DO4_GPIO_Port,DO4_Pin,GPIO_PIN_SET);
HAL_Delay(2000);
HAL_GPIO_WritePin(Temp_PWR_GPIO_Port,Temp_PWR_Pin,GPIO_PIN_SET);//power off Temp PWR
HAL_SPI_MspDeInit(&hspi1);
HAL_GPIO_DeInit(TempAD_CS_GPIO_Port, TempAD_CS_Pin);
SystemClock_Decrease();
HAL_SuspendTick();
HAL_PWREx_EnableLowPowerRunMode();
if(HAL_GPIO_ReadPin(DO4_GPIO_Port,DO4_Pin)!=GPIO_PIN_RESET && a==0)
{
output_flag=1;
a=1;
}
else if(HAL_GPIO_ReadPin(Lock_btn_GPIO_Port,Lock_btn_Pin)!=GPIO_PIN_SET && a==1)
{
a=0;
}
if(output_flag==1)
{
HAL_PWREx_DisableLowPowerRunMode();
SystemClock_Config();
HAL_Init();
HAL_ResumeTick();
MX_GPIO_Init();
huart1.gState = HAL_UART_STATE_RESET;
MX_USART1_UART_Init();
debug("DO4 ON\r\n");
HAL_GPIO_WritePin(Temp_PWR_GPIO_Port,Temp_PWR_Pin,GPIO_PIN_SET);//power off Temp PWR
HAL_SPI_MspDeInit(&hspi1);
HAL_GPIO_DeInit(TempAD_CS_GPIO_Port, TempAD_CS_Pin);
SystemClock_Decrease();
HAL_SuspendTick();
HAL_PWREx_EnableLowPowerRunMode();
output_flag=0;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.